这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-25 / 43

排序:
Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

如何使用 ENA 执行 75 Ω 测量?
您可以将 ENA 的系统特征阻抗变为 75 Ω,然后执行 75 Ω 测量。

FAQ 2015-03-09

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

“电子校准置信度检查”和网络分析仪“系统验证”测试有什么区别?
电子校准置信度检查是测量使用机械校准件或电子校准件进行校准的精度。系统验证测试帮助网络分析仪用户验证他们的网络分析仪是否……

FAQ 2012-12-18

ENA 支持什么机械校准套件和电子校准件?
请参见下面的文档……

FAQ 2012-12-11

ENA 6 系列是否支持用户表征的电子校准件?
不支持。

FAQ 2012-12-10

ENA系列是否允许用户访问误差系数阵列?
ENA矢量网络分析仪系列不允许用户访问误差系数阵列。

FAQ 2012-04-17

如何在是德矢量网络分析仪中进行迹线数学运算?
是德网络分析仪中的迹线数学运算适用于复数实部和虚部数据对。

FAQ 2012-01-11

使用用户定义的校准套件执行校准后,所有记录幅值会显示为-200dB,这是什么原因?

FAQ 2011-10-07

85039B F型校准套件的延迟/直通定义值是否有错误?
定义值没有错误,但测量可插入的被测件时必须修改定义值。

FAQ 2011-10-07

Why isn't calibration option (UK6) available for the 42941A?
The 42941A does not have calibration option because the 4294A specifies total measurement accuracy including the 4294A accuracy.

FAQ 2010-07-12

Why does the DC resistance measurement function of the 4287A require to be calibrated at the same time with Open/Short/Load calibration?
The specified accuracy for the DC resistance measurement is applied when the Open/Short/Load calibration for the DC resistance measurement is performed.

FAQ 2010-07-02

使用 Keysight 16085B 4 终端对至 7mm (APC-7) 适配器时,应使用夹具补偿标准件还是同轴校准标准件?

FAQ 2010-07-02

How should I define or select the residual inductance values of Shorting Bars when performing Short compensation on the E4991A or the 4287A?
Nowadays, the authorized standards stipulate the dimensions of shorting devices and the Short Compensation method which uses the defined inductance values of the shorting devices. It is recommended to consider these authorized standards.

FAQ 2010-07-02

Do the coaxial Short and 50 Ω Load terminations for the 42941A have accuracy specifications?
No, both the coaxial Short and 50 Ω Load standard terminations for the 42941A do not have accuracy specifications.

FAQ 2010-07-02

Can 4263B preserve Open/Short/Load correction data by using Save/Recall function?
No.

FAQ 2010-07-02

Why does measurement data exhibit a discontinuity at 5 MHz or 15 MHz and how can the 4294A get rid of this phenomenon?
The 4294A extends its measurement frequency range up to 110 MHz by terminating each measurement terminal with 50 ohm in order to eliminate the resonance of test leads (including leads inside the 4294A).

FAQ 2010-07-02

4287A 进行接触点检测时显示的 Rdc 测量值不准确,怎样做才能提高其准确度?
执行开路/短路/负载校准和开路/短路补偿。

FAQ 2010-01-26

What is the recommended calibration period of the 16380C?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 42030A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16380A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16190B?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

Is calibration report included in the 16380V-001 Upgrade Kit which adds the 10 µF standard capacitor to the 16380C?
Yes, the 16380V-001 Upgrade Kit includes the 10 µF standard capacitor and its calibration report.

FAQ 2009-06-23

1 2 下一页