Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

126-150 sur 347

Tri:
Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Can the spectrum analyzer mode of the 4395A display noise level below 0.0001 µV / sqrt (Hz) in noise measurement mode?
No, the 4395A can't display noise level below 0.0001 µV / sqrt (Hz) in noise measurement mode.

FAQ 2008-11-16

Is the accuracy of the impedance measurement specified when the 4395A/4396B Option 010 is used with the 87512A?
No, the accuracy of the impedance measurement values obtained by using the 4395A/4396B with the 87512A is not specified.

FAQ 2008-11-16

What does the Input Impedance in Table 11-24 of E4980A User's Guide and Table 39 of E4980A data sheet mean and how should it be applied?
The Table 11-24 and Table 39 describe input impedance of DC bias current monitor.

FAQ 2008-11-12

What is the signal source output impedance of the 4338B?
The signal source output impedance is 1 ohm +/- 0.2 ohms (not specified).

FAQ 2008-11-11

How accurately does the 4338B measure high resistance?
The 4338B accuracy in high resistance measurement is degraded because the maximum measurement range is limited to 100 k ohms.

FAQ 2008-11-11

ESA-L1500A: Spectrum Analyzer Frequency Reference

FAQ 2008-10-08

What is the lowest sampling rate that can be set for the U2300A/U2500A Series USB Data Acquisition (DAQ) devices?
The Keysight U2300A/U2500A Series Data Acquisition (DAQ0 devices can support sampling rates as low as 3Sa/s.

FAQ 2008-09-25

Are the USB data acquisition (DAQ) devices compatible with USB 1.1 or USB 2.0?
The USB data acquisition (DAQ) devices come with Full Speed USB (12Mbps) which is compatible with any USB Host 1.1 and 2.0.

FAQ 2008-09-25

What is the maximum analog output current from the U2300A Series Data Acquisition (DAQ) devices?
The maximum analog output current from the U2300A Series Data Acquisition (DAQ) devices is 5mA.

FAQ 2008-09-25

What is the peak-to-peak voltage of the square wave that is generated by the U1252A Digital Multimeter?
The peak-to-peak value of the square wave that is generated by the U1252A Digital Multimeter is 2.8V.

FAQ 2008-09-24

What programming platforms are compatible with the U2300A Series Data Acquisition (DAQ) devices?
Keysight VEE, LabView, Microsoft Visual Studio and C++ are compatible with the U2300A Series Data Acquisition (DAQ) devices.

FAQ 2008-09-24

Which thermocouple types are compatible with the U2802A Thermocouple input device?
Eight standard thermocouple types defined in the NIST ITS-90 Thermocouple Database are compatible with the U2802A input device….

FAQ 2008-09-24

What are the maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices?
The maximum sampling rates for the U2531A, U2541A and U2542A Data Acquisition (DAQ) devices are:….

FAQ 2008-09-24

What is the maximum frequency that can be measured with the U1252A Digital Multimeter?
The U1252A Digital Multimeter has a frequency counter function that can measure frequency up to 20MHz.

FAQ 2008-09-24

How much internal memory is available to the user in the E363xA and E364xA power supplies?
The E3631A, E3632A, E3633A and E3634A have 3 non-volatile recall states for the output parameters, each of which can store the voltage, current limit and over-voltage protection setting.

FAQ 2008-09-23

66xxA and E36xxA: P-P Voltage Noise Versus RMS Noise
Both Vp-p and Vrms are measures for the unwanted AC components of a DC power supply output. Peak-to-peak noise is measured from the maximum positive point on the waveform to the most negative voltage point.

FAQ 2008-09-22

66xxA and E36xxA: Programmable Current Sinking
In general, current sinking is a fixed value at some percentage of the full scale current output. However, there is an exception for one series of Keysight power supplies. On the 663xB series, the maximum negative current tracks the value programme...

FAQ 2008-09-22

Do the E364xA power supplies have fan cooling?
Yes. The fan speed in the E364xA series supplies is controlled automatically for reduced acoustic noise when the ambient temperature and power supply load is such that the full cooling capability is not required.

FAQ 2008-09-22

What is the signal source output resistance of the 4339B?
The output resistance of DC test voltage source is 1 k ohms ±10 %.

FAQ 2008-09-11

What is the test signal output impedance of the 4294A?
The source output impedance of the 4294A is 25 ohms (nominal value).

FAQ 2008-09-11

What is the output impedance of the E4991A?

FAQ 2008-09-11

What is the Keysight 16065A Bias Voltage Test Fixture maximum DC current specification?
The 16065A maximum dc bias current is not specified. However, based upon the 100 kΩ input resistance,...

FAQ 2008-07-31

Is there any method of measuring impedance at low frequencies below 100 kHz with the 4395A-010?
The option 4395A-010 is designed to measure impedance at frequencies above 100 kHz and, thus it is specified for the range above 100 kHz.

FAQ 2008-06-12

How is measurement accuracy of the E4980A specified when ALC function is set to ON?
Find the test signal level setting in ALC Off mode where the applied signal voltage or current across the DUT is equal to ALC setting value. Then calculate accuracy at this test signal level setting as follows:

FAQ 2008-06-11

Précédente 1 2 3 4 5 6 7 8 9 10 ... Page suivante