这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

201-225 / 347

排序:
What is the sample rate of the Keysight 34401A?
When configured for the fastest reading rate, the 34401A can sample at 1000 readings/second.

FAQ 2005-02-09

Can I use my Infiniium's USB ports and do they support Hi-speed communication?
Depending on the model of Infiniium you have, you may be able to use the USB ports.

FAQ 2004-11-18

8614xA系列和8614xB系列光谱分析仪有何不同之处?
8614xB系列比8614xA系列具有更高的波长精度,以及更快的迹线更新能力。

FAQ 2004-10-28

What is the service level calibration interval for the Keysight E5052A?

FAQ 2004-10-11

What are the TTL input/output levels for the PNA rear panel material handler connection?

FAQ 2004-09-30

Does the Keysight 34401A have a LAN IO Connection?
No. However, if you require Local Area Network (LAN) connectivity, consider the Keysight E5810A LAN-to-GPIB gateway.

FAQ 2004-09-23

Is there any documentation on the 346C - H01 Special Option Noise Source?

FAQ 2004-09-09

我可以为35670A动态信号分析仪使用外置监视器吗?
是,外置VGA监视器可以与新款35670A分析仪一起使用。

FAQ 2004-08-18

What are the sizes and weights of the E8401A, E8403A, and E8404A?
Size and weight information is listed in Appendix A of the E8401A, E8403A User and Service manual.

FAQ 2004-06-28

What are the major differences between the 859xEM EMC Analyzers and the 859xE Spectrum Analyzer families?
The 859xEM EME Analyzer family comes standard with pre-loaded options specifically for EMC precompliance measurements.

FAQ 2004-06-22

Do the 8590EM Series EMC Analyzers have the 1MHz 6dB EMI bandwidth?
Yes, they do....

FAQ 2004-06-22

Is there a replacement for the 85878A EMI Report Generator Software?
Not exactly. See text for further information on this topic....

FAQ 2004-03-30

Why does the N897xA NFA series not show zero after calibration?
The N897xA NFA Series may show a noise figure of a few tenths of a dB which is quite normal.

FAQ 2004-03-30

E1300B: What is the difference between "Peak" and "Dynamic" current in a VXI mainframe?
Peak current is DC. Dynamic current is at 10 khz.

FAQ 2004-02-03

What is the resolution of the SP50?
The pixel size is 20um, with the flexibility for the user to select 10um.

FAQ 2004-01-26

What is the minimum and maximum resolution?
The resolution is always 20um however, the user now has the flexibility to go to 10um if needed.

FAQ 2004-01-26

66xxA, 68xxB 和 N330xA: 功率产品的内存
不同系列的电源产品有不同的存储/调用状态数。

FAQ 2003-11-24

8753,8510,8720: 能不能使用50欧姆网络分析仪测量75欧姆器件?
由于50 ohm测试装置最适合测量50 ohm,因此我们一般不推荐这样做。

FAQ 2003-11-24

8903A, 8903B, 8903E比较
Keysight 是Keysight 8903A的替代产品。

FAQ 2003-11-24

8920A和 8921A之间有什么差别?
8921A是针对蜂窝基站测试客户的解决方案。

FAQ 2003-11-24

在低频率上测量低阻抗器件时阻抗测量的不确定性
对于低频和阻抗应用,与使用反射法的矢量网络分析仪(VNA)相比,使用I-V技术的阻抗分析仪能得到更精确的测量结果。

FAQ 2003-11-24

网络分析仪校准方法比较
参看校准方法比较表

FAQ 2003-11-23

ESG和ESG-D系列: 选择度测量
ESG-D 系列在连续和突发调制模式中提供适宜的邻道功率(ACP)。

FAQ 2003-11-23

SOLT和TRL/TRL*校准之间的差别
矢量网络分析仪要求在误差校正测量前执行测量校准。对于二端口测量,确定响应校准套件的校准算法为SOLT或TRL/TRL*。

FAQ 2003-11-23

What is the minimum noise figure that can be measured using the N897xA NFA Series?
There is no minimum level that can be measured

FAQ 2003-08-26

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页