这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

101-125 / 347

排序:
Do the mean, min, and max values of the InfiniiVision oscilloscopes measurement statistics refer to one signal on the screen or all previously capt...
They refer to the "Count" number of captured waveforms ...

FAQ 2009-03-30

Is the Rdc measurement accuracy of the 4287A better than that of the 4286A?

FAQ 2009-03-13

What benefits can I get by replacing the 4286A with the 4287A?

FAQ 2009-03-11

What is the output impedance of the 4287A?
Nominal output impedance is 50 ohms.

FAQ 2009-03-11

In the arena of using AOI in solder paste inspection, which is more important, repeatability and reproducibility (GR&R) or accuracy?
Different customers put different weight on repeatability and reproducibility (GR&R) versus accuracy.

FAQ 2009-03-01

What is the board weight specification?
For the Series II SP50 and SJ50 systems, the specification is <3kg.

FAQ 2009-02-26

What are the effects of AOI on the environment, for example, does the use of lasers affect the operators?
AOI systems usually have no effect on the PCB or the environment.

FAQ 2009-02-26

What are the advantages and disadvantages of Keysight AOI systems compared to other systems?
The various AOI systems in the market have their unique features but Keysight has a unified platform which protects one's investment.

FAQ 2009-02-26

What is the accuracy on height measurements?
Using the standard calibration plate, typical height bias <3um.

FAQ 2009-02-26

Is there a way to pull the results from my SP50 into a report?
Yes, a reporting package is available on the system.

FAQ 2009-02-26

What are the reasons for choosing an inline solder paste inspection system over an on-board solder paste inspection solution offered on the screen ...
Screen printing with on-board solder paste inspection solutions is typically very slow, so it negatively impacts throughput.

FAQ 2009-02-26

What is our maximum board thickness?
The SP50 Series II standard conveyor accommodates 0.5mm to 4mm (0.02" to 0.157").

FAQ 2009-02-26

What is board size limitation, LXWXT?
The board size that will fit into the SP50 Series II system is 510mmX510mm.

FAQ 2009-02-26

AOI is able to detect solder paste missing or offset but can it detect solder paste volume? And it's height?
The Keysight SP50 is able to test solder paste missing & offset as well as solder paste height and volume.

FAQ 2009-02-25

How do you test solder paste volume and quality, and what are the advantages compared to visual inspection?
Keysight's SP50 solder paste inspection system uses laser inspection to check the solder paste volume, height, area, and offset (all of the print related parameters).

FAQ 2009-02-25

Can the operator access the alarm limits in the SPC software?
Yes, the operator can access the alarm limits in the SPC software.

FAQ 2009-02-25

Are the alarm settings saved in the SPC software?
Yes, the alarm settings are saved in the SPC software.

FAQ 2009-02-25

What units are the area and volume in for the SP50 measurements?
By default the SP50 displays and reports area and volume as normalized percentages.

FAQ 2009-02-25

What is the minimum sensitivity of the N897xA NFA Series?
Sensitivity is not a specified parameter

FAQ 2009-02-09

How can I access to the maximum memory depth (32M/16M) as stated in the U2701A/U2702A Modular Oscilloscope's data sheet?
You can see the effects of maximum memory depth 32/16 Mpts in zoom mode….

FAQ 2009-02-04

Do the U2300A Series USB DAQ devices provide opto-isolation of the analog inputs?
No, the U2300A Series USB DAQ devices do not provide opto-isolation of the analog input channels.

FAQ 2009-02-04

How do I calculate the dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope?
The dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope depends on the error values in the measured value....

FAQ 2009-02-04

What is the output impedance of the 4285A?

FAQ 2009-01-14

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Is the accuracy of the impedance measurement specified when the 4395A/4396B Option 010 is used with the 87512A?
No, the accuracy of the impedance measurement values obtained by using the 4395A/4396B with the 87512A is not specified.

FAQ 2008-11-16

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页