Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-11 of 11

Sort:
Can I operate 86107A over continuous frequency bands?
The 86107A can operate over the following continuous frequency range if the 86100A/B/C mainframe has firmware revision A04.10 or above.

FAQ 2013-12-12

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

What is the equivalent circuit for the 1161A 10:1 passive probe for Infiniium scopes?
The following is an approximation of the equivalent circuit.

FAQ 2010-03-17

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

Do the mean, min, and max values of the InfiniiVision oscilloscopes measurement statistics refer to one signal on the screen or all previously capt...
They refer to the "Count" number of captured waveforms ...

FAQ 2009-03-30

How can I access to the maximum memory depth (32M/16M) as stated in the U2701A/U2702A Modular Oscilloscope's data sheet?
You can see the effects of maximum memory depth 32/16 Mpts in zoom mode….

FAQ 2009-02-04

How do I calculate the dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope?
The dc vertical gain accuracy of a U2701A/U2702A USB Modular Oscilloscope depends on the error values in the measured value....

FAQ 2009-02-04

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Why does the DC Gain Error formula in the DC Gain Accuracy procedure have factors of 0.60 and 0.75 in the DSO80000 Series Infiniiums but not the ot...
These factors are used in the DSO80000 Series Infiniiums because the DC gain is measured with input voltages that are less than full scale, but the spec is relative to a full scale input.

FAQ 2006-10-20

Can I use my Infiniium's USB ports and do they support Hi-speed communication?
Depending on the model of Infiniium you have, you may be able to use the USB ports.

FAQ 2004-11-18