这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-7 / 7

排序:
Will there be specification, performance characteristic or usability differences when using the 11970 Series mixers on the PXA?
Yes, there will be several differences when using 11970 Series mixers with the PXA.

FAQ 2011-04-26

What differentiates a power splitter and power divider and when should one be utilized over the other?
The fundamental difference between power splitters and power dividers (combiners) is the resistor configuration used to separate the power.

FAQ 2010-06-11

各种是德可编程步进衰减器的静态电流消耗是多少?
是德可编程步进衰减器需要 20 mS 的脉冲持续时间,以插入选定的衰减器段。

FAQ 2010-05-14

How do you measure the equivalent output reflection coefficient or equivalent output SWR of a splitter?

FAQ 2009-05-11

It appears there was a specification change for the 355C/D/E/F family of VHF attenuators. Are there additional details?
The specifications were revised in September 1997.

FAQ 2005-03-04

8510: Annual Certification of Calibration Kit

FAQ 2002-06-27

N4261A: On the indicator properties, are the values a peak value or are they peak-to-peak values?

FAQ 2002-06-27