이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 73

정렬방식:
IO Libraries Suite: Keysight IO Libraries Suite에는 무엇이 들어있나요??
Keysight I/O Libraries, Keysight Connection Expert,•I/O 구성 및 문제해결 툴, LXI 기반 계측기를 관리 및 제어할 수 있는 API, 그리고 계측기 드라이버 및 코드 샘플에 대한 빠른 액세스

FAQ 2014-04-07

교정 키트 토크 렌치를 위한 인증(및 재인증) 프로세스는 무엇입니까?

FAQ 2014-03-24

Will there be specification, performance characteristic or usability differences when using the 11970 Series mixers on the PXA?
Yes, there will be several differences when using 11970 Series mixers with the

FAQ 2013-04-26

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

PSA 시리즈 스펙트럼 분석기를 N5530S 측정 수신기 시스템에서 작동시키려면 어떤 옵션이 필요합니까?
옵션 B7J, 옵션 123, 옵션 1DS 및 E4440AU 옵션 233

FAQ 2012-03-15

What field of view (FOV) magnifications are available?
The x6000 does not use the field of view (FOV) concept, it uses an autofocus technique that sizes the inspection image to the joint type being inspected. Several slices are evaluated for the sharpest region to determine the slice location.

FAQ 2012-03-12

Why are my N4010A DEVM test results different with firmware revision A.05.03.15?
Revision A.05.03.15 was a short-lived release that used a modified measurement algorithm. Please upgrade to revision A.05.03.16, which uses the correct measurement algorithm.

FAQ 2011-02-18

IO Libraries Suite: What is new with Keysight IO Libraries Suite 14.0?
Keysight IO Libraries Suite provides a new and improved set of tools for establishing, verifying, and troubleshooting instrument-to-PC connections.

FAQ 2010-10-30

Why does my E6651A fail Source Modulated Power Level Accuracy in TME?
This may be due to a compatibility issue between the E6651A firmware version and TME.

FAQ 2010-10-14

IO Libraries Suite: 지원되는 인터페이스와 작동 시스템은 무엇입니까?
Keysight IO Libraries Support 매트릭스를 확인하십시오.

FAQ 2010-09-08

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

IO Libraries Suite: What has changed in version 14.2?
Version 14.2 includes defect fixes and makes two changes to improve the compatibility of Keysight 488 with third-party software.

FAQ 2010-09-08

IO Libraries Suite: What is the definition of an “Keysight instrument”?
For the purposes of this IO Libraries Suite License Grant, an “instrument” is a device, or a chassis or mainframe that holds such device(s)

FAQ 2010-09-08

What is the static state current consumption for the various Keysight programmable step attenuators?
Keysight Programmable Step Attenuators require a 20 mS pulse duration to engage a selected attenuator section.

FAQ 2010-07-02

어떤 운영 체제가 VEE를 지원합니까?
매트릭스 테이블을 참조하십시오.

FAQ 2010-06-14

전력 스플리터와 전력 분배기의 차이점은 무엇이며 어떤 상황에서 둘 중 하나가 다른 하나보다 우선적으로 사용됩니까?
전력 스플리터와 전력 분배기(결합기)의 근본적인 차이점은 전력 분리에 사용되는 레지스터 구성입니다.

FAQ 2010-06-11

What is the main reason that SMT manufacturers would use solder paste inspection for lead-free paste?
The print process for lead free requires fine tuning such as cycle time modifications, reduction in the aperature-to-pad ratios, squeegee speed/pressure changes, etc.

FAQ 2010-05-19

N5532A 센서 모듈의 주파수 범위는 어떻게 됩니까?
100kHz~4.2GHz, 10MHz~18GHz, 30MHz~26.5GHz 및 30MHz~50GHz.

FAQ 2010-04-13

9kHz까지 E5071C의 저주파수를 포함하는 ECal이 있습니까?
예, N4431B 4포트 ECal은 현재 9kHz까지 지원합니다.

FAQ 2009-11-16

IO Libraries Suite: Keysight IO Libraries 15.0에서는 어떤 프로그래밍 언어를 지원합니까?

FAQ 2009-08-23

How does Keysight specify the bandwidth of the N1021B probe?
The one-way bandwidth of the probe can be estimated using a simplified equation ...

FAQ 2009-06-18

스플리터의 등가 출력 반사 계수 또는 등가 출력 SWR을 측정하는 방법은 무엇입니까?

FAQ 2009-05-11

In the arena of using AOI in solder paste inspection, which is more important, repeatability and reproducibility (GR&R) or accuracy?
Different customers put different weight on repeatability and reproducibility (GR&R) versus accuracy.

FAQ 2009-03-01

What are the advantages and disadvantages of Keysight AOI systems compared to other systems?
The various AOI systems in the market have their unique features but Keysight has a unified platform which protects one's investment.

FAQ 2009-02-26

What is the accuracy on height measurements?
Using the standard calibration plate, typical height bias <3um.

FAQ 2009-02-26

1 2 3 다음