这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 76

排序:
What is the operating temperature range for 34138A test lead set?
The operating temperature range is limited to the DMM model with which it is used....

FAQ 2015-08-21

对校准套件扭力扳手进行认证(和再认证)的过程是怎样的?
目前,是德尚不提供我们的校准套件中包含的任何类型扭力扳手的“数据”。对新采购和再认证的校准套件均是如此。即使是被要求“使用数据校准”时,也不提供扭力扳手的数据。

FAQ 2014-03-24

Can I retrofit option H75 or H76 on my 478A Coaxial Thermistor Mount sensor?
The option H75 and H76 can not be retrofitted on an existing 478A. Either of these options must be ordered at the time the 478A is originally purchased.

FAQ 2013-11-17

86100C 和 86100D 数字通信分析仪的典型功耗是多少?
86100C 和 86100D 典型功耗测量

FAQ 2012-09-25

What Options would my PSA Series Spectrum Analyzer require to operate in an N5530S / N5531S Measuring Receiver system?
It is highly recommended that your PSA have with Option 1DS (100 kHz to 3 GHz Preamplifier) or Option 110 (10 MHz to 26.5 GHz / 50 GHz preamplifier) for improved dynamic range.

FAQ 2012-03-15

What field of view (FOV) magnifications are available?
The x6000 does not use the field of view (FOV) concept, it uses an autofocus technique that sizes the inspection image to the joint type being inspected. Several slices are evaluated for the sharpest region to determine the slice location.

FAQ 2012-03-12

Will there be specification, performance characteristic or usability differences when using the 11970 Series mixers on the PXA?
Yes, there will be several differences when using 11970 Series mixers with the PXA.

FAQ 2011-04-26

Why are my N4010A DEVM test results different with firmware revision A.05.03.15?
Revision A.05.03.15 was a short-lived release that used a modified measurement algorithm. Please upgrade to revision A.05.03.16, which uses the correct measurement algorithm.

FAQ 2011-02-18

IO Libraries Suite: What is new with Keysight IO Libraries Suite 14.0?
Keysight IO Libraries Suite provides a new and improved set of tools for establishing, verifying, and troubleshooting instrument-to-PC connections.

FAQ 2010-10-30

IO Libraries Suite: What is included with the Keysight IO Libraries Suite?
Keysight I/O Libraries, Keysight Connection Expert,I/O Configuration and Troubleshooting Tools, API’s for Managing and Controlling LXI-based Instruments, and Quick Access to Instrument Drivers and Code Samples

FAQ 2010-10-30

Why does my E6651A fail Source Modulated Power Level Accuracy in TME?
This may be due to a compatibility issue between the E6651A firmware version and TME.

FAQ 2010-10-14

IO Libraries Suite: What is the definition of an “Keysight instrument”?
For the purposes of this IO Libraries Suite License Grant, an “instrument” is a device, or a chassis or mainframe that holds such device(s)

FAQ 2010-09-08

IO Libraries Suite: What interfaces and operating systems are supported?
View the Keysight IO Libraries Support matrices.

FAQ 2010-09-08

IO Libraries Suite: What has changed in version 14.2?
Version 14.2 includes defect fixes and makes two changes to improve the compatibility of Keysight 488 with third-party software.

FAQ 2010-09-08

IO Libraries Suite: What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?
The major enhancement that has been added to version 14.1 is compatibility with National Instruments NI-488.2 API or I/O Library.

FAQ 2010-09-08

How wide range of resistivity can the 4339B measure when used with the 16008B?
The 4339B can measure surface resistivity up to 7 x 1017 Ω and volume resistivity up to 8 x 1018 Ω-cm, but it depends on the electrodes of the 16008B used.

FAQ 2010-07-02

VEE支持哪些操作系统?
请参见支持列表。

FAQ 2010-06-14

What differentiates a power splitter and power divider and when should one be utilized over the other?
The fundamental difference between power splitters and power dividers (combiners) is the resistor configuration used to separate the power.

FAQ 2010-06-11

What is the main reason that SMT manufacturers would use solder paste inspection for lead-free paste?
The print process for lead free requires fine tuning such as cycle time modifications, reduction in the aperature-to-pad ratios, squeegee speed/pressure changes, etc.

FAQ 2010-05-19

各种是德可编程步进衰减器的静态电流消耗是多少?
是德可编程步进衰减器需要 20 mS 的脉冲持续时间,以插入选定的衰减器段。

FAQ 2010-05-14

N5532A 传感器模块的频率范围是多少?
100 kHz 至 4.2 GHz,10 MHz 至 18 GHz,30 MHz 至 26.5 GHz 和 30 MHz 至 50 GHz。

FAQ 2010-04-13

有没有可以支持频率低至 9 kHz 的 E5071C 的电子校准?
有,N4431B 4 端口电子校准现在可以支持低至 9 kHz 的频率。

FAQ 2009-11-16

IO Libraries Suite: What programming languages are supported with Keysight IO Libraries version 15.1?
It depends on the API you are using.

FAQ 2009-08-25

与 Keysight 85070E 介电探头套件连用时,各种探头的频率限制及其原因是什么?
通过 3 GHz E4991A 阻抗分析仪,85070E 介电探头选件 020、030 和 050 可拥有最大的频率。

FAQ 2009-06-26

How does Keysight specify the bandwidth of the N1021B probe?
The one-way bandwidth of the probe can be estimated using a simplified equation ...

FAQ 2009-06-18

1 2 3 4 下一页