您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

101-125 / 219

排序:
FAQs: Service Support

FAQ 2008-01-18

FAQs: Error Messages

FAQ 2008-01-18

What is the expected lifetime of the relays used in the Keysight 34970A plug-in modules?
The Keysight 34970A Relay Maintenance System automatically counts the cycles on each relay in the instrument and stores the total count in non-volatile memory on each switch module.

FAQ 2008-01-08

How much torque can I apply to the connectors on my N4011A?
0.9 Nm (approximately 0.66 lb/ft)

FAQ 2007-10-30

How do you install i3070 v7.00 software?
Please follow the instructions in "Installing or Upgrading to Medalist i3070 Software" (E9901-96001).

FAQ 2007-09-12

What is the usage of the "on failure report"?
Allow the user to enter report failures such as 'parallel device' to the particular test.

FAQ 2007-09-12

What is the default directory that i3070 v7.00 installed?
C:\Agilent_ICT.

FAQ 2007-09-12

How does Auto-Guarding select a node for Guarding?
Each Guard node is "weighted" and the priority of which Guard node to use depends on the "weight" given to that node.

FAQ 2007-09-12

What happens to the Agilent3070 directory?
C:\Agilent3070 directory remains so that user’s config and test board directories still prevented.

FAQ 2007-09-12

How do you access the Auto Debug rule editor?
"Actions-Auto Debug-Rule Editor".

FAQ 2007-09-12

Can I run my test program from Agilent3070 directory?
Yes

FAQ 2007-09-12

What should you do prior to executing iVTEP?
"Undo AutoDebug" to enable back all commented pins during VTEP AutoDebug. Enable the commented pins to be debugged using iVTEP.

FAQ 2007-09-12

How to sort the Rule Name according to device types at Rule Database?
Select a device type in Ruleset navigation. Rule Database will show all the rule names that device type selected.

FAQ 2007-09-12

How do you add all the ICT user accounts and groups?
Double click the batch file at "Agilent_ICT\home\system\3070accounts.bat".

FAQ 2007-09-12

What is the short-cut key for "faoff" at Engineer?
Shift+F2.

FAQ 2007-09-12

Why my data didn't get save after edited Lower Tolerance Limit?
After manual edited parameters or options, 'Save Test' combo box must be checked before save.

FAQ 2007-09-12

How to clear Output windows?
Click "View?Engineer?Clear Output" or Use short-cut key "Ctrl+Alt+A".

FAQ 2007-09-12

Where the licenses are stored initially?
"Agilent_ICT\lib\i3070Mux" or "Agilent_ICT\lib\i3070UnMux".

FAQ 2007-09-12

What is the short-cut key to press to do "testhead power on"?
Ctrl-Shift+P.

FAQ 2007-09-12

Why the commands that I type not supported in command line?
User can "filter off" to enable back filtered commands. But software may fail due to some commands are not supported.

FAQ 2007-09-12

How to pause test execution queue?
Click "Pause" button.

FAQ 2007-09-12

What is the short-cut key to press to "login" to Engineer Test?
F9.

FAQ 2007-09-12

Where is the "switch" application located?
C:\Agilent_ICT\util\switch.

FAQ 2007-09-12

What is "RunAllAIC"?
All unpowered analog tests will be executed based on AIC list. "Fail" result will be displayed only as "RED" color.

FAQ 2007-09-12

How to display short format for the Column Name?
Click "Edit-Preferences", go to Engineer Test Tab, select "Short" and click OK.

FAQ 2007-09-12

上一個 1 2 3 4 5 6 7 8 9 下一頁