这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

201-219 / 219

排序:
Keysight E4418A/E4419A功率计支持终止的日期是什么时候?
E4418A和E4419A功率计在2004年3月1日到了保证的最低5年支持终止日期。是德现在只能提供“尽力而为”的维修服务。

FAQ 2004-07-26

Can the line module in my EPM/EPM-P series power meter be replaced at my local Service Center?
This will depend on the model number and the date of manufacture.

FAQ 2004-07-12

为什么每次在重新引导系统时16700系列逻辑分析仪上都显示错误时间?
时间错误最常见的原因是CPU中的电池电量不足。可以把设备送到本地服务中心,更换电池。也可以参阅服务手册,自己更换电池。

FAQ 2004-06-10

如果16700系列逻辑分析仪在重装过程中发生错误或中断怎么办?
在发出设备维修前,请检验BIOS设置是否正确

FAQ 2004-06-09

为什么16700系列分析仪不能正确引导?
16700的BIOS设置是否正确?有时用户会选择"DEFault" (默认的) BIOS设置,以解决问题,但这些设置并不正确。

FAQ 2004-06-08

Can high contact resistance be repaired?
Switching 120 mA 10-100 times may clean the contacts.

FAQ 2004-05-14

What is the 8590 series product history?
A complete listing of 8590 series models that include their frequency range, introduction date, discontinuance date, end of support date, and model replacement if applicable.

FAQ 2004-04-06

34970A: Can I buy fuses for the 34970A or 34901A from Keysight or locally?
Yes. Fuses for the 34970A or 34901A can be purchased from Keysight or an outside hardware store.

FAQ 2004-02-05

How can the memory in a 437B Power Meter be erased for security purposes?
This can be done by a sequence of keypresses, or by a sequence of remote commands.

FAQ 2004-02-05

What are the mean time between failure (MTBF) and mean time to repair (MTTR) estimates for the 33120A?
Mean time between failure (MTBF) is 40,000 hours. Mean time to repair (MTTR) is 1.2 hours.

FAQ 2003-06-03

What type of memory is used in the 3499A/B/C?
Flash Memory is used to store 3499A/B/C configuration and set-up.

FAQ 2003-06-02

Is support included with iDEN® FTA for Windows?
Detailed setup and operating instructions will be included with your shipment.

FAQ 2003-01-24

What are the benefits of using relay-cycle-counters provided by the 3499A/B/C?
In a high-speed automated test equipment (ATE) system, unplanned downtime can be fatal to a production line.

FAQ 2003-01-22

Does the 3488A and/or 3499A/B/C contain batteries?
There are no batteries in the 3488A. For the 3499A/B, please check the firmware revision.

FAQ 2002-09-23

How do I determine the firmware revision of the Keysight 3499A/B/C?
From the front panel, press the "MENU" button, scroll to find the "revision info" in the menu list, press the "ENTER" button.

FAQ 2002-09-23

If a customer wants to increase the number of N2280A/N2281A channels, do they have to buy an additional 3499 mainframe and module?
You can install two of the N2280A and/or N2281A modules in the 3499A mainframe.

FAQ 2002-09-23

The E8404A Enhanced Monitor provides many history features: minimum and maximum values, histograms, operating times, and event logs. What are they ...
The history features provide you with insight into the trends of your test system. Without any programming on your part, your VXI test system will be monitored and information stored.

FAQ 2002-09-17

What is the relay used on the 44470A/D?
The relay supplier and part number for the 44470A is "OMRON" type is G6AK-274P. There is not a Keysight 4 x 4 part number.

FAQ 2002-09-06

8566/68AB: What Is the Part Number for the IF Interconnect Cables?

FAQ 2002-06-27

以前 1 2 3 4 5 6 7 8 9