这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-20 / 20

排序:
Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

Can I order the replacement part of 16089E's clips?
When the clip is faulty, please proceed to place a new order on 16089E or purchase the spare Kelvin Clip Leads.

FAQ 2013-03-17

能否在 ENA 中禁用或启用 Windows 的自动登录功能?
能。为了在无域系统中禁用或启用 Windows 的自动登录功能,请执行以下步骤:

FAQ 2012-12-18

“电子校准置信度检查”和网络分析仪“系统验证”测试有什么区别?
电子校准置信度检查是测量使用机械校准件或电子校准件进行校准的精度。系统验证测试帮助网络分析仪用户验证他们的网络分析仪是否……

FAQ 2012-12-18

在Keysight ENA和ENA-L系列矢量网络分析仪上,如何确定硬盘版本?

FAQ 2011-10-07

How can I replace the contact tip of the 16334A?
The replacement contact tip is orderable by part number 16334-09002.

FAQ 2010-07-02

4284A LCR 表和 42841A 偏置电流源及 42842A/B 夹具一起使用时,需要注意哪些问题?

FAQ 2010-05-12

如何订购 Keysight 42941A 阻抗探头的替换探针?
订购部件编号为 42941-60004 的是德产品

FAQ 2010-03-16

What is the recommended calibration period of the 16380C?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16190B?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 42030A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16380A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

How can I replace the contact electrodes of the 16118A?
The contact electrodes of the 16118A cannot be replaced by user.

FAQ 2009-01-13

Is the collet (center contact) of the 16454A identical to that of the 42942A (part number 1250-0907)?
Yes, When replacing the collet (center contact) of the 16454A, you can use the same part (part number 1250-0907) as that used in the 42942A.

FAQ 2009-01-12

Does the part number 16334-09002, which is described in the 16334A operation and service manual, indicate one unit of the part?
Yes, the part number 16334-09002 indicates one unit of the part.

FAQ 2009-01-12

Can I order separately the clip leads and probe leads included in the 16338A?
Yes, the respective clip leads, probe lead and mating cable of the 16338A can be ordered by part numbers.

FAQ 2008-07-02

How can I order supplemental parts for component test fixtures/accessories?
You can order the necessary parts by the part numbers shown in the Accessories Selection Guide for Impedance Measurements.

FAQ 2008-04-22

在Keysight 4291A/B阻抗分析仪上,能否使用标准网络分析仪校准套件来执行测试探头校准?
只有使用为的4291A/B提供的校准标准件,才能在Keysight 4291A/B阻抗分析仪上进行测试探头校准。

FAQ 2007-05-29

My Keysight 4284A / 4285A LCR Meter is indicating an "ADC ERR" error message. What are the corrective actions?
The error message is an indication that the LCR meter's A/D converter within the measurement circuit is malfunctioning.

FAQ 2007-05-03