検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

コンテンツのタイプ

製品カテゴリ

226-250 / 573

並べ替え
Is there any sample program for the 4395A to measure THD (Total Harmonic Distortion)?
Yes, a free sample program (HP BASIC/ IBASIC) for the 4395A to measure THD is available on Keysight.com.

FAQ 2008-11-16

What kind of benefits does the 4395A's file transfer function have?
The "File Transfer Function" of the 4395A allows you...

FAQ 2008-11-16

Can I get any instrument driver (a Plug & Play driver) for the 4395A?
No, instrument driver for the 4395A is no longer supported and is currently unavailable. Please use GPIB commands to control the 4395A.

FAQ 2008-11-16

What is the objective of "Auto On/Off" command for setting DC Bias ranging mode of the E4980A via GPIB?
The "Auto On/Off" command enables the bias voltage range to be fixed at +/-40 V range (when Auto Off command is executed). DC bias voltage can be varied from 0 V to +/-40 V with a constant 5 mV resolution at the fixed 40 V range.

FAQ 2008-11-12

What should I perform when the E4980A settings cannot be remotely controlled in Web server (Web browser) control mode?
It is caused by a problem on the cash file of proxy server or on the browser of your PC. In order to enable the control, try reloading the latest cash file by pressing the right button of your mouse and clicking update function label.

FAQ 2008-11-12

What can the E4980A's GPIB command ":BIAS:RANGe:AUTO" be used for?
The :BIAS:RANGe:AUTO command enables the DC Bias voltage range to be fixed at +/-40 V range (when :BIAS:RANGe:AUTO OFF command is executed).

FAQ 2008-11-12

What kinds of instrument drivers support the E4980A?
The following instrument drivers are available as of October 2008.

FAQ 2008-11-12

Can I program a secondary parameter (such as D, Q, Rs, etc) for the list sweep setup of the E4980A?
Yes, when the list sweep setup is programmed over GPIB, the secondary parameter can be set by using SCPI commands.

FAQ 2008-11-12

NFAシリーズ雑音指数アナライザで、オートレンジ・モードでRFアッテネータ・レンジを問い合わせることはできますか?
オートレンジ・モードでKeysight NFAのRFアッテネータを問い合わせるコマンドを以下に示します

FAQ 2008-10-13

What digital communication I/O Options are available with the E7400A Series EMC Analyzers?
See content for details...

FAQ 2008-10-09

Is any Visual Basic or C sample program for the 4263B available?
No, all the 4263B sample programs can only be used in the HP Basic for Windows operating environment.

FAQ 2008-09-24

Which delimiter should be used for programming the 4263B data output over GPIB?
LF (line feed) and EOI (end of identify) signal (in the 4263B operation manual, it is described as " ^END") should be used.

FAQ 2008-09-24

34405AをHyperTerminalから制御することができますか?
いいえ。

FAQ 2008-09-23

U2300シリーズでは、他にどのようなソフトウェアを使用できますか?
Keysight VEE、LabView、Microsoft Visual Studio、C++ を使用できます。

FAQ 2008-09-22

U2300シリーズがLabViewで動作するには、どのドライバが必要ですか?
U2300シリーズがLabViewで動作するにはIVI-COMドライバが必要です。

FAQ 2008-09-22

U1250シリーズ・ハンドヘルド・マルチメータでデータ・ロギングする場合、標準的なUSBケーブルを使用できますか?
いいえ。

FAQ 2008-09-22

E363xA and E364xA: Compatibility with National GPIB I/F Card
Yes, the National Instruments GPIB board is very configurable. However, this can cause some problems.

FAQ 2008-09-22

HyperTerminalは、U1251A/U1252Aで使用できますか?
いいえ。

FAQ 2008-09-22

U1241A/U1242A を PC に接続できますか?
いいえ。U1241A/U1242A には PC インタフェースが装備されていません。

FAQ 2008-09-22

U2300/U2500シリーズDAQデバイス用のサンプル・プログラムはありますか?
はい。

FAQ 2008-09-22

What conditions cause the 4339B to return the measurement status code 5 in response to "FETCh?" command
Refer to Note in Appendix C of the 4339B Operation Manual for the definition of measurement status codes.

FAQ 2008-09-11

4294A sample programs don't work and error 173 "Active/System controller required." is displayed. How can I fix this symptom?
Since the SYSTEM ID of the 4294A has changed, depending on the firmware version, the program lines which refer to the SYSTEM ID needs to be modified.

FAQ 2008-09-11

How should the frequency characteristics simulation data be read after the command "SIMFCHAR" is sent to the 4294A?
Since the frequency characteristics simulation data is saved in the memory trace data, "OUTPMTRC?" command should be used to read out the memory trace data (complex values) for all the frequency points.

FAQ 2008-09-11

Is an I-Basic program available for performing constant current measurement with the 4294A?
The I-Basic program for constant current measurement is described on the 4294A Programming Manual.

FAQ 2008-09-11

Keysight PNA / PNA-Lシリーズ・ネットワーク・アナライザのプログラミング時、エラー103を表示されます。どうしてですか?
+103, CALC measurement selection set to none

FAQ 2008-09-02

前へ 1 2 3 4 5 6 7 8 9 10 ... 次へ