検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

コンテンツのタイプ

製品カテゴリ

201-225 / 572

並べ替え
How Can I Remotely Determine the Serial Number and Firmware Revision of My Test Set?

FAQ 2009-06-11

Is there an example program for acquiring data from the Keysight 8970B Noise Figure meter via the GPIB bus?
Vee program found here...

FAQ 2009-04-28

How do I connect my InfiniiVision oscilloscope directly to a PC via the LAN interface?
To establish a point-to-point LAN connection, you will need either a PC with an Auto-MDIX network adapter or a crossover (not straight-through) LAN cable.

FAQ 2009-04-23

NFA シリーズ雑音指数アナライザから雑音指数および利得データを収集するためのサンプル・プログラムはありますか?
はい

FAQ 2009-04-16

16500 シリーズ・ロジック・アナライザの設定を 16900 シリーズ・ロジック・アナライザの設定に変換できますか?
はい、ただし、一部のモジュールのみです。

FAQ 2009-03-30

Why Can’t I Open the BenchLink II AgtDB.mdb Database File in Microsoft® Access?
The file is password protected to prevent any changes to be made to the file.

FAQ 2009-03-13

Can the IBasic option be retrofitted on the Keysight E5100A/B Analyzers?
Unfortunately, for those E5100A/Bs ordered with option UKR (delete internal IBasic) there is no retrofit to reinstall IBasic in the instrument.

FAQ 2009-03-12

Is it possible to create a VBA, LabVIEW or any control program for application and run it on the 4287A?

FAQ 2009-03-11

Do the 4284A GPIB commands comply with SCPI?
Yes. The GPIB programming language of the 4284A is SCPI.

FAQ 2009-03-11

Can I use any instrument driver software for the 4284A?
National Instrument’s LabVIEW driver supports the 4284A.

FAQ 2009-03-11

Are the GPIB commands of the 4287A compatible with the 4286A?

FAQ 2009-03-11

When using a U2701A/U2702A USB Modular Oscilloscope, what is the maximum data point of the waveform that I can save ?
When using a U2701A/U2702A USB Modular Oscilloscope, you can save a maximum of 2000 data points for a single channel measurement….

FAQ 2009-02-11

Can open/short/load correction data be entered in the 4285A from an external PC over GPIB?

FAQ 2009-01-14

Can I use any instrument driver software for the 4285A?

FAQ 2009-01-08

How can I clear an error message shown on the display of the 4294A/4395A/4396B by using GPIB command?
Send the "KEY 18" command to the instrument.

FAQ 2009-01-08

Can the time stamp function and :LIST:SEQuence:TSTamp:DATA command of the E4980A be used for a list sweep measurement in STEP mode?
No, the time stamp function can be used in the sequential (SEQ) mode only.

FAQ 2009-01-08

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

Can I write my own measurement personalities or downloadable programs (DLPs) for the E4406A, PSA Series, or ESA Series Analyzers?
No. We do, however, offer many tools to facilitate remotely interfacing of our instruments to a PC to write custom applications. We do also offer flexible digital demod through the 89601A software, and this software does have custom macro capabi...

FAQ 2008-11-21

Keysight PNAシリーズ・ネットワーク・アナライザで、メモリ・トレースからASCIIテキスト・ベースのデータ・ファイルを作成できますか?
PNAのメモリ・トレースをテキスト・ファイルに直接出力できないため、以下のプロセスのいずれかを使用する必要があります。

FAQ 2008-11-20

I use Keysight VEE and Labview and would like instrument drivers for the E4406A, PSA Series, ESA Series, and EMC Series. Where can I download VXI ...
The E4406A, PSA Series, ESA Series, and EMC Series new IVI-Com drivers as well as the older VXI Plug and Play drivers are available in the "Drivers and Software" section for each product.

FAQ 2008-11-20

For the E4406A and PSA Series, what are the advantages of using a USB connection or a LAN connection [10 Base T] instead of a GPIB connection?
For large block data transfers, USB is faster than LAN, and LAN is faster than GPIB. The 89601A VSA link to the E4406A and PSA Series transfers large blocks of data and data speed becomes important. USB is faster than LAN, and much fater than GPI...

FAQ 2008-11-20

Do you have a GPIB command comparison chart between the 4195A and the 4395A?
Yes, please refer to 4195A-4395A GPIB Command Correspondence Table.

FAQ 2008-11-17

What kind of benefits does the 4396B's file transfer function have?
The "File Transfer Function" of the 4396B allows you...

FAQ 2008-11-17

Can the spectrum analyzer mode of the 4396B measure the power of a digital modulation signal such as QAM?
Yes, but it works only when the signal is periodic and the 4396B with option 4396B-1D6 (Time-gated spectrum analysis) is used.

FAQ 2008-11-17

Is there any sample program for the 4395A to measure THD (Total Harmonic Distortion)?
Yes, a free sample program (HP BASIC/ IBASIC) for the 4395A to measure THD is available on Keysight.com.

FAQ 2008-11-16

前へ 1 2 3 4 5 6 7 8 9 10 ... 次へ