Technical Support
Electronic Measurement
Refine the List
By Topic
-
All Topics
- Programming & Data Transfer
By Type of Content
- FAQ (512)
By Product Category
1-25 of 512
FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers
FAQ 2020-02-24 |
|
Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.
FAQ 2020-02-06 |
|
Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.
FAQ 2016-07-08 |
|
Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.
FAQ 2016-07-08 |
|
Which PNA / ENA remote interfaces support use of the Keysight cXL code translator?
On the PNA and ENA vector network analyzers, the Keysight cXL code translator is supported and operational only via the GPIB interface.
FAQ 2016-01-27 |
|
Does FieldFox support data-based cal kits?
FAQ for FieldFox support of Cal Kits
FAQ 2015-09-09 |
|
When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.
FAQ 2014-08-11 |
|
How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file
FAQ 2014-03-13 |
|
On the Keysight NFA Series of Noise Figure Analyzers, is it possible to query the RF attenuator range while in the auto range mode?
The command to query the Keysight NFA RF attenuator while in the auto ranging mode is: DIAG:BLU:RF:RANG?
FAQ 2014-01-31 |
|
Is there a sample program for acquiring Noise Figure and Gain Data from the NFA Series of Noise Figure Analyzers?
Yes
FAQ 2014-01-31 |
|
How can I save my log plot data to a CSV file type when using the option 226 Phase Noise personality on the PSA or ESA?
In the Phase Noise personality, the log plot data can only be saved as a binary file with the .lpt extension.
FAQ 2014-01-31 |
|
Which currently available power meters are compatible with the 8753E network analyzer?
In order to work with the 8753E network analyzer, your power meter must emulate either the 436A, 437B, 438A E4418A or the E4419A power meter. Keysight is no longer selling those power meters. However, the E4418B (formerly named the EPM-441A) and E4...
FAQ 2013-11-17 |
|
Can I use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters?
No, you cannot use a normal USB cable for datalogging with the U1250A Series Handheld Digital Multimeters…..
FAQ 2013-11-17 |
|
Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.
FAQ 2013-11-17 |
|
Can HyperTerminal be used with the U1251A/U1252A Handheld Digital Multimeter?
No, HyperTerminal cannot be used with the U1251A and U1252A Digital Multimeter….
FAQ 2013-11-17 |
|
Can HyperTerminal be used with the 34405A Digital Multimeter?
No, HyperTerminal cannot be used with the 34405A Digital Multimeter….
FAQ 2013-11-17 |
|
Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....
FAQ 2013-11-17 |
|
Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....
FAQ 2013-11-17 |
|
How do I re-install the default waveform files for the CXG/EXG/MXG vector series signal sources?
The arbitrary waveform files are stored in the non-volatile memory of these signal sources when they ship out of the factory. In case these waveform files are accidentally deleted, a user can retrieve them through either of the following methods...
FAQ 2013-08-14 |
|
How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.
FAQ 2013-06-25 |
|
How do I remotely program my spectrum or vector signal analyzer?
Instructions, examples, and references for remotely programming your spectrum analyzer
FAQ 2013-05-16 |
|
What USB storage devices are compatible with the MXG?
The MXG is now compatible with most USB storage devices.
FAQ 2013-03-13 |
|
How do I configure RS-232 for communications on my 53131/32A or 53181A frequency counter?
None of the counters can communicate over RS-232. Frequency counters must use GPIB to communicate with the PC. RS-232 is used for printing only.
FAQ 2013-02-07 |
|
Is it possible to programmatically receive the displayed low/high stimulus values when using the "CALC1:MARK:BWID:DATA?" bandwidth query results?
When manually configuring the ENA network analyzer via the Marker – Marker Search – Bandwidth ON, the manual process results in low and high stimulus values as displayed on the analyzer’s front panel.
FAQ 2012-12-20 |
|
What is the process to capture a trace image to the floppy disk on the Keysight 8712ES/ET and 8714ES/ET Vector Network Analyzers?
The 8712ES/ET and 8714ES/ET Vector Network Analyzers support HPGL, PCX, PCL5, and GIF image saves via the floppy drive.
FAQ 2012-12-11 |
|