这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

26-50 / 514

排序:
我能在 FieldFox 上使用局域网连接吗?
可以。请阅读情景介绍。

FAQ 2012-06-01

How do I remotely make an Adjacent Channel Power (ACP) measurement with the 89601A VSA software using Microsoft Excel?
Click here for information on controlling the 89601A software using Excel to make an ACP measurement.

FAQ 2012-05-29

How do I remotely read the summary table for a demodulated Wireless LAN signal from the 89601A VSA software using Microsoft Excel?
Open the Excel file provided, select "Enable Macros" and follow procedure documented inside spreadsheet.

FAQ 2012-05-29

How do I remotely program my PSA Series Spectrum Analyzer or E4406A VSA Series Analyzer to read ASCII trace points without using an instrument driv...
Click here for an example demonstrating how to over LAN read ASCII trace points of an entire EDGE waveform in the GSM w/ EDGE personality Power Vs. Time measurement.

FAQ 2012-05-29

How do I remotely read status bits and set interrupts for the 89601A VSA software using Microsoft Excel?
Save the self-extracting archive to disk, open it and click unzip to extract the 89600_Status_Bits.xls and ACP.sdf files to your C:\temp directory.

FAQ 2012-05-29

How do I remotely read demodulated symbols from the 89601A VSA software using Microsoft Excel?
Click here for information on reading demod symbols from the 89601A software using Excel.

FAQ 2012-05-29

How do I remotely program my PSA Series Spectrum Analyzer or E4406A VSA Series Analyzer to transfer Raw I/Q trace data using the IVI-COM driver in...
Click here for information on transfering Raw I/Q trace data using IVI-COM and .NET.

FAQ 2012-05-29

How do I remotely transfer screen images from my E4406A VSA Series Analyzer using Visual Basic 6?
Click here for information on transfering screen images.

FAQ 2012-05-28

What file formats does the 89601A VSA software support for signal waveforms?
Recorded data from the following files can be interpreted by the 89600: ASCII (.txt and .csv), Binary (89600 SDF .sdf, .dat), Binary (E3238 .cap), Binary (N5510A .bin), MATLAB 7 (or earlier, .mat)

FAQ 2012-05-28

For my ESA/PSA/EMC Series Spectrum Analyzer or E4406A VSA Series Analyzer how do I serial poll to determine when an auto-alignment is complete usin...
Click here for information on performing an alignment and using serial polling to determine when it is complete.

FAQ 2012-05-28

How do I remotely program my E4406A VSA Series Analyzer to transfer binary block data in Visual Basic 6?
Click here for information on transfering binary block trace data.

FAQ 2012-05-28

How do I remotely transfer screen images from my ESA/PSA Series Spectrum Analyzer using Visual Basic 6?
Click here for information on transfering screen images.

FAQ 2012-05-28

What is required to use Remote UI for the E4991A?
You need to prepare the following items: the E4991A, a PC, the E4991A VBA software (E4991A_vba.msi) included in the furnished CD-ROM and, LAN environment. For details, please refer to chapter 10 "Using LAN" of the E4991A operation manual.

FAQ 2012-05-10

Can we upgrade N5181A or N5182A first-generation MXG to an N5181B or N5181B MXG X-Series signal generator?
No, there is not a hardware upgrade path from the first-generation MXG to MXG X-Series signal generator.

FAQ 2012-04-30

ENA 6 系列的代码是否兼容 871x 系列?
不兼容,但可使用 871x 至 ENA 6 系列代码转换套件来辅助代码转换。

FAQ 2012-04-17

能否在 ENA 上生成标准文件?

FAQ 2012-04-17

用户能否在 ENA 6 系列上运行由 ENA 7 系列创建的 VBA 程序?
用于 ENA 7 系列的 VBA 程序不能在 ENA 6 系列上运行。但是通过导出和导入某些模块,用户也可以使用这个程序。

FAQ 2012-04-17

ENA系列是否允许用户访问误差系数阵列?
ENA矢量网络分析仪系列不允许用户访问误差系数阵列。

FAQ 2012-04-17

How do I transfer the current Signal List in my E7400A EMC Analyzer to my PC using remote commands?
First save the list to a file inside the instrument and then transfer the file.

FAQ 2012-03-16

如何使用电脑上的VEE软件远程操作ESA、EMC或者PSA系列频谱分析仪将屏幕图像导入文件?
如欲了解详情,请参见上下文……

FAQ 2012-03-16

When using a PSA cellular measurement personality, what are the commands to set the external RF Attenuation parameter for the mobile or base station?
External RF Attenuation is found under the Input/Output hardkey. The corresponding SCPI commands are...

FAQ 2012-02-28

How do I remotely program my PSA Series Spectrum Analyzer to capture the equivalent learn string?
Click here to download a VEE example program for capturing and restoring the instrument state.

FAQ 2012-02-25

How can I transfer trace data from the 89400 VSA to my PC?
The VSA always saves data in standard data format; the utility is run from the DOS prompt.

FAQ 2012-02-25

What is the correct cable to use with the ESA Series for RS-232 communication?
Part number RS232-61601

FAQ 2012-02-25

手持式频谱分析仪的远程控制命令是否兼容任何其他仪器?
手持式频谱分析仪的远程控制命令集兼容其他频谱分析仪的命令集。

FAQ 2012-02-20

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页