Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-24 из 24

Упорядочить:
Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....

FAQ 2013-11-17

How do I transfer waveforms, screen images, and measurements from my InfiniiVision oscilloscope to a PC using IntuiLink Data Capture?
Keysight’s free IntuiLink Data Capture software provides an easy way to transfer deep-memory waveform data, screen images, and measurements from your oscilloscope to your PC via the USB, LAN, or GPIB interface.

FAQ 2011-06-06

How do I save a screen image from my 5000/6000/7000-series InfiniiVision oscilloscope to a USB storage device?
These instructions assume that your scope has system software version 05.00 or later (see Utility | Service | About Oscilloscope -> System version to see your scope’s version).

FAQ 2010-09-15

VEE Pro: Why can't I talk to an instrument at GPIB address 21?
The reason is that each device on the GPIB has to have a unique address, including the computer's GPIB card.

FAQ 2010-09-09

In the programming for the U2701A and U2702A Modular Oscilloscopes, why do I sometimes get a different waveform…
In programming the U2701A/U2702A Modular Oscilloscopes, the waveform is different from the Measurement Manager's (AMM) because....

FAQ 2010-08-09

Can I program a waveform captured by my oscilloscope into a Keysight arbitrary waveform generator?
Yes. The free IntuiLink Waveform Editor software will download waveform data from Keysight Infiniium, 6000 series, and 54600 series oscilloscopes and send the data to the a Keysight 33120A, 33210A, 33220A, or 33250A generator.

FAQ 2010-05-14

Keysight Infiniium Oscilloscopes: Programming the Oscilloscope
Use the example programs and programming manual available for download from this web site.

FAQ 2009-12-11

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

Where to find the USB modular scopes IVI-COM programming guide?
download the programming guide.

FAQ 2009-09-29

How can I save comma separated variable (CSV) data to my USB thumb drive?
Set this up in Utility -> Print Config.

FAQ 2009-08-17

How do I save deep memory waveform data from my InfiniiVision oscilloscope to a USB storage device?
Use half-channel mode and ASCII XY, ALB, or BIN format. Within the "Save" menu, press Settings and select the max number of points. Make sure you are at a slow enough time/div setting that all the points are on screen, and then ...

FAQ 2009-05-03

How do I connect my InfiniiVision oscilloscope directly to a PC via the LAN interface?
To establish a point-to-point LAN connection, you will need either a PC with an Auto-MDIX network adapter or a crossover (not straight-through) LAN cable.

FAQ 2009-04-23

Where can I find the U2701A/U2702A IVI-driver's programming reference guide?
The U2701A/U2702A IVI-driver's reference guide is in "Documentation" in the Keysight IVI driver folder upon completion of driver installation

FAQ 2009-04-21

Are there any programming commands for the U2701A/U2702A USB Modular Oscilloscope?
Yes, the IVI driver is available for the U2701A/2702A USB Modular Oscilloscope instrument control….

FAQ 2009-04-21

Are there any SCPI programming commands available for the U2701A/2702A USB Modular Oscilloscope instrument control?
No, there are no SCPI commands available for the U2701A/2702A USB Modular Oscilloscope….

FAQ 2009-04-21

When using a U2701A/U2702A USB Modular Oscilloscope, what is the maximum data point of the waveform that I can save ?
When using a U2701A/U2702A USB Modular Oscilloscope, you can save a maximum of 2000 data points for a single channel measurement….

FAQ 2009-02-11

How can I access to the maximum memory depth (32M/16M) as stated in the U2701A/U2702A Modular Oscilloscope's data sheet?
You can see the effects of maximum memory depth 32/16 Mpts in zoom mode….

FAQ 2009-02-04

Can I automatically position the Y1 and Y2 cursors to the voltage values at X1 and X2?
Yes, using SCPI remote programming commands, follow these steps...

FAQ 2008-09-30

What options do the DSO3000-series oscilloscopes offer for saving data?
You can save data to internal oscilloscope memory or you can use the N2860A Scope Connect software to save data to your PC.

FAQ 2008-09-30

Keysight BenchLink XL 54600 Scope Toolbar: Failed Instrument Search

FAQ 2003-09-12

Keysight Infiniium Oscilloscopes: What Is the Format for Learn Strings?

FAQ 2003-08-01

Keysight Infiniium Oscilloscopes: Does the Keysight Infiniium Oscilloscope Work With VEE?

FAQ 2003-08-01