Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 43

Упорядочить:
How many Keysight 34970A data acquisition units can be connected to a single PC at a time?
Only one Keysight 34970A can be connected for each RS-232 port on the PC. A GP-IB cable can be used to connect up to 15 units if the GP-IB cable is being referenced by the VEE software. The Benchlink Data Logger 3 software can support up to 4 units...

FAQ 2012-01-25

Can Excel control a scan, and make and record measurements using the 34970A?
Use the 34970A IntuiLink add-in, Excel Macro language, or the Instrument Code Wizard.

FAQ 2011-12-20

The Benchlink Data Logger Software is unable to see my 34970A even though it is connected, how do I correct this?

FAQ 2011-12-20

What is the data transfer rate of PXI, PXIe, and AXIe?
PXI-1 has two variants...

FAQ 2010-10-06

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

VEE Pro: Why can't I talk to an instrument at GPIB address 21?
The reason is that each device on the GPIB has to have a unique address, including the computer's GPIB card.

FAQ 2010-09-09

Can I retrieve data from the 34970A while it is scanning?
No. You can collect data during a scan, stop the scan and then transfer the data.

FAQ 2010-09-09

How can I make NI LabVIEW communicate with my 82357A USB/GPIB Interface?
Install the IO libraries Suite and configure the 82357A. There may be other configuration steps if you install NI-VISA.

FAQ 2010-08-30

How can I remotely view what modules are installed in the 34970A?
Use the SYSTem:CTYPe? {100|200|300} SCPI command or System.CardType( ) IVI COM object.

FAQ 2010-05-16

Can the measurements taken be read from the 34980 Data Acquisition Front Panel?
No

FAQ 2010-05-14

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

How much of data points from my data acquired can I save into one file?
What we observed is that if you log your file into *.csv file, the most no. of points you will be capturing is 65536 points. However, if you are saving into *.txt file, it will depend on the type of...

FAQ 2009-09-29

IO Libraries Suite: Is there any other software that needs to be installed when I am using an application that utilizes NI-488.2 and Keysight IO Lib...
It depends if there is third party connectivity hardware or software installed.

FAQ 2009-08-25

Why Can’t I Open the BenchLink II AgtDB.mdb Database File in Microsoft® Access?
The file is password protected to prevent any changes to be made to the file.

FAQ 2009-03-13

What programming platforms are compatible with the U2300A Series Data Acquisition (DAQ) devices?
Keysight VEE, LabView, Microsoft Visual Studio and C++ are compatible with the U2300A Series Data Acquisition (DAQ) devices.

FAQ 2008-09-24

What are the drivers needed to run the U2300A Series Data Acquisition (DAQ) devices with LabView?
The IVI-COM driver is required for the U2300A Series Data Acquisition (DAQ) devices to work with LabView.

FAQ 2008-09-24

Are there any sample programs provided for the U2300A and U2500A Series Data Acquisition (DAQ) devices?
Yes, sample programs of VEE, LabView and Microsoft® Visual Studio® are available for the U2300A and U2500A Series Data Acquisition (DAQ)….

FAQ 2008-09-24

Can Excel control a scan, and make and record measurements using the 34980A?
Use the 34980A IntuiLink add-in or the Excel Macro language.

FAQ 2007-01-22

How do I disable the front panel display on the 34970A Data Acquisition Unit in order to achieve the maximum scanning speed for measurement?
This cannot be done via the front panel controls, it can only be done remotely via the Benchlink Data Logger II Software or programmatically.

FAQ 2007-01-10

What is the maximum number of readings you can obtain from the 34970A directly?

FAQ 2007-01-10

Can the measurements be displayed on the 34980 front-panel?
No.

FAQ 2007-01-10

34970A: How do I confirm that my RS-232 cable is working properly?
By placing a short on one end of the RS-232 cable and connecting the other to a PC, you can use Hyperterminal to verify if the cable is working properly.

FAQ 2006-08-29

How can I download/upload configuration to/from the 34970A?
Follow the procedures below to download and upload configuration to and from 34970A.

FAQ 2006-02-28

How can I test the RS-232 connection on my 34970A?
RS-232 connection problems can be in the instrument settings, the instrument COM port hardware, the cable connectors and wiring, the PC COM port and in the program setting.

FAQ 2006-02-02

1 2 Следующие