Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-25 из 74

Упорядочить:
When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

Is it possible to programmatically receive the displayed low/high stimulus values when using the "CALC1:MARK:BWID:DATA?" bandwidth query results?
When manually configuring the ENA network analyzer via the Marker – Marker Search – Bandwidth ON, the manual process results in low and high stimulus values as displayed on the analyzer’s front panel.

FAQ 2012-12-20

What is required to use Remote UI for the E4991A?
You need to prepare the following items: the E4991A, a PC, the E4991A VBA software (E4991A_vba.msi) included in the furnished CD-ROM and, LAN environment. For details, please refer to chapter 10 "Using LAN" of the E4991A operation manual.

FAQ 2012-05-10

Does the ENA allow user access to the Error Coefficient Arrays?

FAQ 2012-04-17

Is the ENA 6 series code compatible with the 871x series?
No, but 871x to ENA 6 series code conversion kit is available to assist the code conversion.

FAQ 2012-04-17

On the ENA 6 series, can I run a VBA program which is made on the ENA 7 series?
A VBA project for the ENA 7 series doesn't work on the ENA 6 series as is. However, the program is likely to work with exporting and importing of the modules.

FAQ 2012-04-17

Is it possible to generate touchstone files on the ENA?

FAQ 2012-04-17

What is an alternative solution to the 87075C / 87050E replacement?
Build your home-made switch box using the L4491A RF/MW switches. Refer to the application note for details.

FAQ 2012-01-11

Does the ENA support 87050E / 87075C series multiport test sets?
Unlike the E5061A and E5062A, the E5061B, E5071C and E5072A (ENA) does NOT support full functions of 87050E / 87075C. But it is possible to change switch state of 87050E-Hxx / 87075C-Hxx via GPIB.

FAQ 2012-01-11

Are the commands compatible between the ENA and the ENA-L?
Yes. Commands for the ENA / ENA-L are fully compatible as far as the common functions are concerned.

FAQ 2011-10-07

On the ENA and ENA-L, is there a SCPI command to query the active trace?
Yes.

FAQ 2011-10-07

On the ENA / ENA-L, what is the meaning of "1.#QNB" or "1.#QNAN"?

FAQ 2011-10-07

What are the equations that relate Real and Imaginary data pairs to Log Magnitude, Polar, Phase, and Smith Chart formats?

FAQ 2011-10-07

On the ENA and ENA-L, is there a SCPI command to query the active channel?
Yes.

FAQ 2011-10-07

While programming the ENA I am receiving the error, "-128, Numeric data not allowed". Why?
For many analyzers the data transfer format is adjustable when outputting data...

FAQ 2011-10-07

Is there a Keysight VEE Sample program outlining use of an SRQ to programmatically detect completion of an ECal Calibration Process?
Yes.

FAQ 2011-10-07

How do I configure my Keysight IO Libraries Suite 14 to communicate with my ENA via LAN?

FAQ 2011-10-07

Is it possible to control external instruments by the ENA/ENA-L?
Yes. It is possible to control external instruments by the ENA/ENA-L with built-in VBA programs.

FAQ 2011-10-07

Are there equation examples for ENA Equation Editor?
Yes.

FAQ 2011-10-07

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

On the ENA / ENA-L, how do I exclude the soft keys when saving the screen image?

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

Is there an outline for configuring my HP Basic to communicate with the Keysight ENA analyzer via SCPI-LAN?

FAQ 2011-10-07

Using the VBA program, can the ENA / ENA-L control the handler interface to control other peripherals?
Yes.

FAQ 2011-10-07

Is the ENA code-compatible with the 8753?
No, but the Code Conversion Assistant Editor is available to assist with code conversion.

FAQ 2011-10-07

1 2 3 Следующие