这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-25 / 74

排序:
When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

Is it possible to programmatically receive the displayed low/high stimulus values when using the "CALC1:MARK:BWID:DATA?" bandwidth query results?
When manually configuring the ENA network analyzer via the Marker – Marker Search – Bandwidth ON, the manual process results in low and high stimulus values as displayed on the analyzer’s front panel.

FAQ 2012-12-20

What is required to use Remote UI for the E4991A?
You need to prepare the following items: the E4991A, a PC, the E4991A VBA software (E4991A_vba.msi) included in the furnished CD-ROM and, LAN environment. For details, please refer to chapter 10 "Using LAN" of the E4991A operation manual.

FAQ 2012-05-10

用户能否在 ENA 6 系列上运行由 ENA 7 系列创建的 VBA 程序?
用于 ENA 7 系列的 VBA 程序不能在 ENA 6 系列上运行。但是通过导出和导入某些模块,用户也可以使用这个程序。

FAQ 2012-04-17

ENA系列是否允许用户访问误差系数阵列?
ENA矢量网络分析仪系列不允许用户访问误差系数阵列。

FAQ 2012-04-17

ENA 6 系列的代码是否兼容 871x 系列?
不兼容,但可使用 871x 至 ENA 6 系列代码转换套件来辅助代码转换。

FAQ 2012-04-17

能否在 ENA 上生成标准文件?

FAQ 2012-04-17

Does the ENA support 87050E / 87075C series multiport test sets?
Unlike the E5061A and E5062A, the E5061B, E5071C and E5072A (ENA) does NOT support full functions of 87050E / 87075C. But it is possible to change switch state of 87050E-Hxx / 87075C-Hxx via GPIB.

FAQ 2012-01-11

What is an alternative solution to the 87075C / 87050E replacement?
Build your home-made switch box using the L4491A RF/MW switches. Refer to the application note for details.

FAQ 2012-01-11

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

Is it possible to control external instruments by the ENA/ENA-L?
Yes. It is possible to control external instruments by the ENA/ENA-L with built-in VBA programs.

FAQ 2011-10-07

存储屏幕图像时,如何关闭ENA/ENA-L上的功能键?

FAQ 2011-10-07

ENA方程编辑器(Equation Editor)有提供方程范例吗?
是的。 方程范例在如下的文件"EquationEditor_Examples.txt"中有。..

FAQ 2011-10-07

在 ENA 和 ENA-L 上是否有查询活动通道的 SCPI 命令?

FAQ 2011-10-07

我该如何配置Keysight IO程序库套件14,以便通过局域网与ENA进行通信?

FAQ 2011-10-07

While programming the ENA I am receiving the error, "-128, Numeric data not allowed". Why?
For many analyzers the data transfer format is adjustable when outputting data...

FAQ 2011-10-07

What are the equations that relate Real and Imaginary data pairs to Log Magnitude, Polar, Phase, and Smith Chart formats?

FAQ 2011-10-07

在 ENA 和 ENA-L 上是否有查询活动迹线的 SCPI 命令?

FAQ 2011-10-07

Is there an outline for configuring my HP Basic to communicate with the Keysight ENA analyzer via SCPI-LAN?

FAQ 2011-10-07

ENA 代码是否兼容 8753?
否,但代码转换辅助编辑器可帮助进行代码转换。

FAQ 2011-10-07

ENA系列网络分析仪上的"1.#QNB"和"1.#QNAN"代表什么意思?

FAQ 2011-10-07

ENA 和 ENA-L 的编程指令可以互相兼容吗?
是的

FAQ 2011-10-07

Using the VBA program, can the ENA / ENA-L control the handler interface to control other peripherals?
Yes.

FAQ 2011-10-07

有没有Keysight VEE示例程序概括说明如何使用SRQ通过程序来检测ECal校准过程是否完成?
有。

FAQ 2011-10-07

1 2 3 下一页