Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 281

Sort:
Why does handheld scope’s date/time display disappears or shows hexa characters?
This condition indicates that the internal memory battery level is low.

FAQ 2013-11-22

Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

Can I use the MXA or PXA real-time Frequency Mask Trigger (FMT) to provide a trigger output that can be used to trigger another device?
Yes, you can configure the MXA or PXA to provide a trigger output when using FMT.

FAQ 2013-08-07

Can I get the real-time I/Q samples out via LAN on my MXA or PXA signal analyzer with option RT1 or RT2?
No, however you can save the real-time trace (Frequency & Amplitude) data into a .csv file from the spectrogram trace (10,000) traces.

FAQ 2013-08-07

Are the Keysight 531xxA and 53200 Series frequency counter inputs floating or grounded?
The counter inputs are not floating -- the BNC shield (shell) is at chassis ground (earth ground).

FAQ 2013-02-07

The trigger signals between the E1476B and the external voltmeter need to be routed through the E8491B. Can you provide the commands for the routi...
The trigger path between the external voltmeter and the E1476A is channeled through the E8491B...

FAQ 2013-01-04

Does Keysight offer any application notes that discuss the theory of Time Domain Reflectometry (TDR) measurements?
Keysight provides Application Note 1304-2, "Time Domain Reflectometry Theory".

FAQ 2012-11-05

How to calculate the bit clock frequency under DSI interface of U8903A?
The Bit clock frequency can be calculated by multipling the number of channels,bit length and frame clock frequency.

FAQ 2012-08-25

What is the maximum bit clock cycle per frame for DSI interface of U8903A?
64 bit clock cycle per frame.

FAQ 2012-07-25

Can the 8657x Signal Generator be turned on with the RF output off?
No, it can't. When a DUT could be destroyed by high RF output.

FAQ 2012-06-08

What is the measurement uncertainty for the 8902A Option 50?
The only uncertainty in the 8902A Option 050 test system should be the accuracy of the attenuation source.

FAQ 2012-05-30

What is the CDMA Codogram display on the E7495A/B Wireless Base Station Test Set?
Codogram is a three dimensional display of Walsh code versus time versus code power. Click here for more details.

FAQ 2012-05-29

How do I optimize my cdmaOne ACPR measurement for the third offset (2.75 MHz offset, 1 MHz bandwidth) in the E4406A and PSA Series cdmaOne personal...
By changing the default number of FFTs segments to 5 and upgrading to the 14 bit digital IF (E4406A only) you can substantially improve your results.

FAQ 2012-05-28

Where can I find technical overviews and self-guided demonstrations of the E4406A and PSA Series measurement personalities?
Technical overviews are available for the following personalities: GSM/EDGE, cdma2000, 1xEV-DO, W-CDMA, cdmaOne, NADC/PDC, Phase Noise (PSA/ESA), and Noise Figure (PSA).

FAQ 2012-05-28

What cdmaOne (Option BAC) radio standards and band classes are supported by the E4406A and PSA Series for the ACP and Spur Close measurements?
Radio standards IS-95A, J-STD-008, IS-97D and IS-98D are supported. The following Band Classes are supported to comply with IS-97D and IS-98D requirements: Band Class 0 (800MHz), Band Class 1 (1900MHz), Band Class 3 (JTACS), Band Class 4 (Korean ...

FAQ 2012-05-28

What are the measurement intervals for the W-CDMA, cdma2000, and 1xEV-DO QPSK EVM measurements for E4406A and the PSA Series? Is the 12.2k Reverse ...
Click on this FAQ to get detailed information on the measurement interval ranges.

FAQ 2012-05-28

Which Application Notes are Most Relevant to the PSA Series Spectrum Analyzer?
This page contains links to application notes that are relevant to PSA Series spectrum analyzers.

FAQ 2012-05-11

Why is the measured PCS band PvT mask position -6 dBc for -10 us, Mobile Station Transmit power levels 11-15, instead of following the ETSI 11.10 s...

FAQ 2012-03-02

How do I correct for external harmonic mixer conversion loss with a PSA Series Spectrum Analyzer (E4440A, E4446A, E4448A)?
The PSA series provides the ability to compensate for conversion loss. You can use one of four amplitude correction factor registers. The correction factors are entered using amplitude/frequency pairs.

FAQ 2012-02-28

How do I remove signal images from the display of the PSA Series Spectrum Analyzer (E4440A, E4446A, E4448A)?
The PSA uses a signal identification process called image suppression. This process removes the images from the display leaving only true signal.

FAQ 2012-02-28

Do I need a bias tee or a diplexer for the 11970 or 11974 series harmonic mixers?
Neither the 11970 or 11974 Series requires a bias tee or diplexer.

FAQ 2012-02-28

Can I do time gating with my PSA Series Spectrum Analyzer?
Yes, click here for additional information

FAQ 2012-02-27

What is the frequency range of the N5532A Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

What do the terms "time gating", "gated video", "gated FFT" and "gated sweep" mean in the PSA Series Spectrum Analyzer?
Time Gating is a tool used in Spectrum Analysis to eliminate the transient effects of a pulsed RF signal when the user wishes to observe the signal itself. There are three basic types of Time Gating. Click here for additional information.

FAQ 2012-02-26

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

1 2 3 4 5 6 7 8 9 10 ... Next