Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-11 из 11

Упорядочить:
Why does handheld scope’s date/time display disappears or shows hexa characters?
This condition indicates that the internal memory battery level is low.

FAQ 2013-11-22

Does Keysight offer any application notes that discuss the theory of Time Domain Reflectometry (TDR) measurements?
Keysight provides Application Note 1304-2, "Time Domain Reflectometry Theory".

FAQ 2012-11-05

Can U1602A/B and U1604A/B measure capacitance of 0.13nF?
Based on the datasheet, for 0.13nF, it falls in the range of 60nF. To calculate the range of fluctuation of the reading,…

FAQ 2010-12-20

What is the best way to ensure simultaneous triggering of multiple units of modular products?
Using the cardcage, U2781A is the best way of ensuring simultaneous triggering of multiple units

FAQ 2010-12-20

VEE Pro: Why can't I talk to an instrument at GPIB address 21?
The reason is that each device on the GPIB has to have a unique address, including the computer's GPIB card.

FAQ 2010-09-09

How do I convert *.svw file to *.csv file in PC Link for U160xA/B?
1) From within PC Link, click on the "Load SVW" icon on the tool bar...

FAQ 2010-07-18

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

What is the equivalent circuit for the 1161A 10:1 passive probe for Infiniium scopes?
The following is an approximation of the equivalent circuit.

FAQ 2010-03-17

What is the update rate for U1600A series handheld scope?
update rate is 14 waveforms per second

FAQ 2009-08-06

Why does handheld scope’s DMM measurement frequently stall after one hour of continuous operation?
This condition indicates that the internal memory battery level has dropped to 1.4V or lower.

FAQ 2009-07-16

How can I declassify the 83480A or 54750A Memory?
Press: Utility (Hardkey) > System Config... (Softkey) > Declassify Frame Memory (Softkey)

FAQ 2005-05-02