Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-24 of 24

Sort:
The trigger signals between the E1476B and the external voltmeter need to be routed through the E8491B. Can you provide the commands for the routi...
The trigger path between the external voltmeter and the E1476A is channeled through the E8491B...

FAQ 2013-01-04

VEE Pro: Why can't I talk to an instrument at GPIB address 21?
The reason is that each device on the GPIB has to have a unique address, including the computer's GPIB card.

FAQ 2010-09-09

The E8404A Enhanced Monitor makes many measurements. How do I access this information about the mainframe?
Many of the measurements taken are displayed in abreviated format on the front panel display.

FAQ 2002-09-17

Has latency improved in the Keysight E8491B compared to the Keysight E8491A?
No. It still requires 100-200 microseconds per E8491B transfer.

FAQ 2002-09-17

When I switch the E8404A front panel fan switch to its VAR position, I am handing control of the mainframe's fans over to the Enhanced Monitor. Hav...
No, you have not. The Enhanced Monitor will control the fan based on your instructions issued to it through the slot temperature limits you set.

FAQ 2002-09-17

What Is OHCI?
Open Host Computer Interface (OHCI) is defined by the IEEE-1394 trade association.

FAQ 2002-09-17

Can I tell the E8404A Enhanced Monitor to take a measurement?
No. The Enhanced Monitor monitors over 80 signals throughout the mainframe every two seconds.

FAQ 2002-09-17

Why are there two temperature limits per slot on the Keysight E8404A?
The two limits really have two different jobs.

FAQ 2002-09-17

The OHCI PC Plug-in card includes a power cable that ships with a E8491B. What does the power cable do?
The power cable supplies the host PC power which is required by the OHCI card.

FAQ 2002-09-17

On the E8404A why doesn''t the fan return to "65%" level when I turn the fan switch to FULL and then back to VAR in an empty frame?
The Enhanced Monitor's fan controller is always concerned about rapid temperature increases.

FAQ 2002-09-17

Will applications written using the E8491A run using the E8491B?
Yes.

FAQ 2002-09-17

What are key factors that make the E8491B faster than the E8491A?
New OHCI, PC plug-in cards include 2 kbyte buffers. This is 4 times larger than previous cards' 500 byte buffer. So, each transfer can be 4 times larger.

FAQ 2002-09-17

Can the E8491B VXI-Firewire interface be used in multiple-card cage configurations?
The E8491B can be used in multiple-card cage systems. There are, however, certain limitations.

FAQ 2002-08-14

Is the E8481A register-based or message-based?

FAQ 2002-06-27

E1332A: Reciprocal Counter for (Freq/Per)

FAQ 2002-06-27

What is E1472A mode of E8482A?

FAQ 2002-06-27

E1445A: Generating Multiple Tone Waveforms

FAQ 2002-06-27

Is E8482A register-based or message-based?

FAQ 2002-06-27

Is E8483A register-based or message-based?

FAQ 2002-06-27

E1332A, E1333A: Work Around for Instrument Hanging When Frequency=0

FAQ 2002-06-27

What is the function of the downloadable channel list in E8481A?

FAQ 2002-06-27

Is E8480A register-based or message-based?

FAQ 2002-06-27

What is the function of the E8480A "Emergency Reset"?

FAQ 2002-06-27

E1445A Sine Wave Limitation Using ARM:LAY1:COUNT

FAQ 2002-06-27