Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-7 из 7

Упорядочить:
What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

How can I calculate the equivalent phase delay, as a function of frequency, for a given electrical delay as set on Vector Network Analyzer?
Equivalent phase delay, based upon electrical delay is computed as: θ˚ = Ftest * Delay * 360

FAQ 2011-10-07

When measuring a capacitor via a Keysight LCR meter, what is the best circuit mode, Cs or Cp?
To measure L, C, or R, there are two equivalent circuit models.The LCR meter can select the mode by setting the FUNC (function) to Cp, Cs, Lp or Ls.

FAQ 2010-09-30

E4991A-002/4291A/B-002 with 16454A: Why is impedance measurement value different from the value calculated from permeability?
Error compensation in the permeability measurement firmware produces the difference between measured impedance and permeability.

FAQ 2010-07-02

Does typical permittivity measurement accuracy includes all the uncertainties due to the E4991A with opt 002, 16453A and MUT insertion conditions?
Yes. All the uncertainties are included in the typical measurement accuracy.

FAQ 2010-07-02

Does the 4338B have 4-terminal pair measurement circuit configuration?
No. The 4338B has a shielded 4-terminal measurement circuit configuration.

FAQ 2008-06-12