这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-7 / 7

排序:
如果在是德矢量网络分析仪上设定了电延迟,如何通过频率计算等效相位延迟?
根据电延迟,等效相位延迟可通过公式: θ˚ = Ftest * Delay * 360计算

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

When measuring a capacitor via a Keysight LCR meter, what is the best circuit mode, Cs or Cp?
To measure L, C, or R, there are two equivalent circuit models.The LCR meter can select the mode by setting the FUNC (function) to Cp, Cs, Lp or Ls.

FAQ 2010-09-30

Does typical permittivity measurement accuracy includes all the uncertainties due to the E4991A with opt 002, 16453A and MUT insertion conditions?
Yes. All the uncertainties are included in the typical measurement accuracy.

FAQ 2010-07-02

E4991A-002/4291A/B-002 with 16454A: Why is impedance measurement value different from the value calculated from permeability?
Error compensation in the permeability measurement firmware produces the difference between measured impedance and permeability.

FAQ 2010-07-02

Does the 4338B have 4-terminal pair measurement circuit configuration?
No. The 4338B has a shielded 4-terminal measurement circuit configuration.

FAQ 2008-06-12