您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

226-250 / 331

排序:
How can I update the MWA software on my ENA to the latest revision?
The latest revision of the MWA can be downloaded from Keysight web page.

FAQ 2009-07-15

How do I configure the ESA-E Series Spectrum Analyzer to make Bluetooth® Measurements?
The ESA-E Bluetooth measurement personality Option 228 is available to make Bluetooth measurements.Click here for additional information.

FAQ 2009-06-17

Why can't I order upgrade option 304, Bluetooth® bundle any longer?
Options within the bundle MUST be ordered individually. Click here to see the option listing for the equivalent 304 bundle.

FAQ 2009-06-17

If I already have an E4438C-406 Bluetooth® license, can I upgrade to N7606B Signal Studio Software Bluetooth® without any extra charges?
Yes, you can upgrade to the N7606B Signal Studio Software free of charge.

FAQ 2009-06-09

How do I download my preferred Quick Help language for my U1602A/U1604A Handheld Oscilloscope?
Download your preferred Quick Help language for the U1602A and U1604A Handheld Oscilloscope from the Product Reference CD……

FAQ 2009-05-03

How do I resolve Error 631/Error 635 when it appears on the display of the 34405A Digital Multimeter during self-test?
You can resolve Error 631/Error 635 on the 34405A Digital Multimeter by performing a firmware upgrade….

FAQ 2009-03-25

How can I order the upgrade kit of the 4287A?

FAQ 2009-03-11

Why must my instrument firmware be A.05.03.12 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during Feb 2009.

FAQ 2009-03-09

Will all versions of the Keysight Logic Analyzer application run on Windows® 2000?
No, the highest version supported under Windows 2000 is 3.67.1009. Use 3.80.0002 or higher for Windows XP SP3 or Windows Vista.

FAQ 2009-02-17

How can I order the upgrade kits for the 4285A?
The available upgrade kits are listed on the 4285A Option Upgrades page, which is linked to Keysight LCR Meters Upgrades homepage.

FAQ 2009-01-14

Why is an incorrect version of Signal Studio N7613A, N7612B, and N7606B shown when I use the “Add or Remove Programs” window in “Control Panel” on ...
This Signal Studio version number discrepancy can be ignored, please proceed with your application removal. This error will be corrected with the next version roll.

FAQ 2008-12-02

How can I order the upgrade kits of the 4396B?
The model numbers of available upgrade kits for the 4396B options are as follows.

FAQ 2008-11-17

Can the E4980A with option E4980A-005 be upgraded to standard model?
Yes. The E4980A-005 can be upgraded to the standard model by ordering the E4980AU-007 Upgrade Kit. The upgrade can be performed at Keysight service center only.

FAQ 2008-11-12

How can I upgrade my E4438C with option 418, Signal Studio for HSDPA over W-CDMA, to option 419, Signal Studio for 3GPP W-CDMA HSPA?
In order to upgrade an E44438C with option 418 to option 419, you need to purchase E4438CK-419 and upgrade the firmware of the E4438C to version C.04.95 and above.

FAQ 2008-10-28

Can you add 1MHz frequency on E4981A-002?
Yes, the upgrade product E4981AU-001 is available.

FAQ 2008-10-20

What digital communication I/O Options are available with the E7400A Series EMC Analyzers?
See content for details...

FAQ 2008-10-09

Which firmware revision displays the identity of Hewlett Packard or Keysight Technologies for the E4418 and E4419B Power Meters?
For the E4418B, the firmware revision A1.08.01 and older will display Hewlett-Packard in the IDN queries…..

FAQ 2008-09-25

Is it possible to retrofit the 4263B with option 002?
No, there is no upgrade path for retrofitting the 4263B with 20 kHz test frequency option.

FAQ 2008-09-24

How can I order the 4294A option upgrade kit?
The 4294A option upgrade information is available from the Impedance Analyzers Upgrades page.

FAQ 2008-09-11

The sensitivity of the ENA rotary knob is too precise to set long electrical delay.
Please update your ENA firmware to the A.09.10 or later.

FAQ 2008-09-10

How many measurement personalities will fit onto the flash memory of my E4406A VSA Series Analyzer?
The E4406A began shipping in December 2003 with 64 MB flash memory, which fits all measurement personalities at the same time. A memory calculator is available to help you determine which options can be loaded together with the 48 MB flash memory...

FAQ 2008-08-28

Is it possible to upgrade my DSO6000 Series oscilloscope to a MSO model?
Yes, by purchasing one of these upgrade kits ...

FAQ 2008-08-01

與測試或實驗室應用軟體相容的硬體版本為何?
您的 E5515C 硬體與應用軟體版本需滿足下列連結表格所述的要求。

FAQ 2008-07-30

I can't order 16340A CR BOX which is necessary for the performance test of 4339B and 4349B. How can I get 16340A?
The replacement CR box is the combination of 16353A, 16353H and 42038A.

FAQ 2008-07-04

Which front panel RF connector option should I order for the N9039A RF Preselector?
That would depend on the input connector type of the PSA being used in the system. See FAQ content for details...

FAQ 2008-07-01

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁