Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 35

Упорядочить:
Can you advise of alternatives to printing and acquiring screen images from the various Keysight Analyzers equipped with only a GP-IB interface?
There are several way to retrieve screenshots.

FAQ 2014-02-18

What Printers can be used for my Network and Spectrum Analyzer products?
Printer Compatibility Information for your specific model of Network and/or Spectrum Analyzer can be found here.

FAQ 2014-01-31

What is the process to capture a trace image to the floppy disk on the Keysight 8712ES/ET and 8714ES/ET Vector Network Analyzers?
The 8712ES/ET and 8714ES/ET Vector Network Analyzers support HPGL, PCX, PCL5, and GIF image saves via the floppy drive.

FAQ 2012-12-11

What is the frequency range of the N5532A Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

Can I hide the softkey menu when I perform "Dump Screen Image" on the ENA / ENA-L?
Yes.

FAQ 2012-02-02

Is it possible to improve the print speed of my ENA?
Yes

FAQ 2011-10-07

Can I modify the trace background color from black to white on the ENA?

FAQ 2011-10-07

What printers are supported by the X-Series (PXA/MXA/EXA/CXA) Signal Analyzers?
Any Windows XP compatible printer.

FAQ 2010-05-16

Can I print the graph data to a printer?
Yes. On a graph tab, click the Preferences... button and select Show Graph Menu Bar.

FAQ 2010-05-05

Printer Setup with the Keysight 8920A,B, 8921A with Firmware Below A.14.00

FAQ 2009-06-11

Is it possible to plot Noise Figure and Gain traces from the 8970B to a printer via the Intelligent Interfaces Converter?
Yes, as long as the converter can still be purchased.

FAQ 2009-04-28

Which printers are supported by the InfiniiVision oscilloscopes?
Here is a list of tested printers and other printers that are likely to work...

FAQ 2009-04-15

Screen Dumped color (HP-GL format) does not always match the display color on the 4396B LCD. Is this normal?
Yes, it is normal because the HP-GL does not have any color information.

FAQ 2008-11-17

What options do the DSO3000-series oscilloscopes offer for saving data?
You can save data to internal oscilloscope memory or you can use the N2860A Scope Connect software to save data to your PC.

FAQ 2008-09-30

What will occur if I use non-recommended printers with the ENA / ENA-L?
Some printer drivers may cause malfunctions...

FAQ 2007-09-12

Is there a master listing of compatible printers for various network analyzers and impedance analyzers?

FAQ 2007-07-10

Why won't my LaserJet printer print from the oscilloscope's USB port?
Connect the oscilloscope to the printer's parallel port using a USB to Parallel Port adapter.

FAQ 2007-02-20

Can I connect a printer directly to the Keysight 34970A?
Although you cannot connect a printer directly to the Keysight 34970A, you can use the Keysight BenchLink Data Logger software to acquire...

FAQ 2005-05-11

How can I remotely capture the screen image of an 8560 Series Spectrum Analyzer?
See the attached example VEE program...

FAQ 2003-11-04

Keysight 8902AT, Vectra, Viper and Plotter Configurations

FAQ 2003-11-04

Keysight Infiniium Oscilloscopes: Why Won't My Thinkjet Work?

FAQ 2003-08-01

Can I Use a Plotter with the 892NX Test Sets?

FAQ 2002-06-27

8757: Printing from 8757D with Microprint 50 and Laserjet 5

FAQ 2002-06-27

8920, 8921 Centronics Printer Support

FAQ 2002-06-27

8711 Family: Compatible Printers

FAQ 2002-06-27

1 2 Следующие