这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

76-100 / 110

排序:
Why are measurement values inaccurate when the 16089B is used with the 4338B?
It is recommended that the 16005B (Part Number 16005-60011) be used in place of the 16089B.

FAQ 2008-11-11

Can I use all fixtures and accessories that I'm using with the 4268A and the 4288A?
Yes, they can be used with E4981A.

FAQ 2008-10-20

How can a normal type BNC connector be connected to the 4339B's high voltage BNC connector?
Normal type BNC connector should not be used because it does not have the withstanding voltage rating enough for the application of 4339B's test voltage output up to 1000 V dc.

FAQ 2008-09-11

Would you give me any information about A1 analog board's part number changes?
04263-66501(Original) => 04263-66511, 04263-66521(Enhancement)*1 => 04263-66531

FAQ 2008-07-29

In the 4263B service manual, there is not a part number of the BNC connector for Ext Trigger. What is the P/N?
It is not prepared the service parts as BNC connector, since it is solodered on PCA directly.

FAQ 2008-07-07

Can I order separately the clip leads and probe leads included in the 16338A?
Yes, the respective clip leads, probe lead and mating cable of the 16338A can be ordered by part numbers.

FAQ 2008-07-02

The key cap of the power switch tends to come unfastened. What measure can I take to meet the situation?
It is recommended to replace with 0371-3953.

FAQ 2008-06-30

Would you give me the information on part number changes for the mechanical parts?
Please refer to the following table.

FAQ 2008-06-29

What is the part number of the black padding (bezel) between the CRT and sub front panel?
The part number is 04194-25002, which is used to protect the CRT from dust.

FAQ 2008-06-27

How would I distinguish between old EEPROM (PN 1818-5719) and new one (PN 5183-4149) when transferring the EEPROMs to new CPU board?
It can be distinguished with the manufacturer part number on the top of the EEPROMs.

FAQ 2008-06-27

Has the part number of H.V. Block Assembly (HVR and FBT) been changed?
Yes. It is changed from 9100-4695 to 9100-5273.

FAQ 2008-06-27

What is the difference between 16190A and 16190B? Can 16190B be used for 4291A/B?
16190B is calibrated up to 3GHz, and 50 ohm termination applicable up to 6GHz. The 16190B can be used 4286A, 4291A/B too.

FAQ 2008-06-27

What is part numbers for LCD assemblies compatible with A91 LCD modules (P/N: 04278-61102 or 04278-61103)?
Please check the following table.

FAQ 2008-06-27

What is the part number of the GPIB I/F?
Parts number is E4970-66533.

FAQ 2008-06-27

Why does the probe pin bend a little?
The bend prevents the pin hall.

FAQ 2008-06-27

What is a part number of the new GP-IB Assembly and ROM set?
New GP-IB assembly iis 04284-66520, and it is workable from FW Rev.03.20.

FAQ 2008-06-27

Is the 16196D included in the fixture selection menu of the 4287A?
No. Please use "SETUP USER FIXTURE" key of the 4287A to register the model number and electrical length (27.3 mm) of the 16196D.

FAQ 2008-06-11

Why are 4339B measurement values unstable when measuring resistance above 100 GΩ with the 16117B or 16118A test fixture?
Resistance above 100 GΩ is beyond the measurable range of the 16117B/16118A.

FAQ 2008-06-11

Can the 4263B with Option 4263B-001 measure transformer parameters without using the 16060A?
Yes, but you need to change DUT connections when measuring parameters for the secondary of transformer after measuring for the primary.

FAQ 2008-06-11

Is electrical length compensation required when using RF coaxial test fixture with the E4980A?
No, the electrical length compensation for RF coaxial test fixtures is not required.

FAQ 2008-06-11

What is the replacement of 16143B?
The replacement of 16143B is Keysight part 16143-60011.

FAQ 2008-06-11

Can I use the 4338B with test fixtures and test leads which are designed for use with LCR meters?
Yes, SMD test fixtures such as the 16044A and test leads such as the 16048A which are designed for use with LCR meters can be used with the 4338B.

FAQ 2008-06-11

Can I use non-Keysight resistivity test fixtures with the 4339B?
Yes, as long as the resistivity test fixture has connectivity to the 4339B, it can be used with the 4339B. It is recommended that the 16117C test leads be used to connect a non-Keysight test fixture.

FAQ 2008-06-10

Is there any test fixture for the 4339B to measure SMD components at test voltages above 100 V dc?
The 16339A Component Test Fixture is available.

FAQ 2008-06-10

How can the 4294A apply a DC bias voltage over 40V to DUT?
An external DC source and a protection circuit need to be used with the 4294A to apply a DC bias voltage over 40V. For biasing axial and radial lead type DUT, the 16165A with a built-in protection circuit is available.

FAQ 2008-05-26

以前 1 2 3 4 5 下一页