这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

26-50 / 110

排序:
The 4395A with the 41800A Active Probe or the 41802A 1 MΩ Input Adapter: Is any calculation required for converting the data for 50 Ω input?
No, any conversion calculation related to the difference in input impedance (between 1 MΩs and 50 Ωs) is not required. You can directly read the measurement value on the 4395A.

FAQ 2010-07-02

Can the 4294A measure a grounded DUT?
The 4294A can measure the grounded DUT when used with the 42941A Impedance Probe.

FAQ 2010-07-02

Is there any effective way to measure the impedance of a pressure sensitive SMD component (ex. a ferrite bead) with the 16196 series or 16197A test...
In order to measure a pressure sensitive device, the pressure applied to the DUT by the test fixture needs to be carefully controlled.

FAQ 2010-07-02

How wide range of resistivity can the 4339B measure when used with the 16008B?
The 4339B can measure surface resistivity up to 7 x 1017 Ω and volume resistivity up to 8 x 1018 Ω-cm, but it depends on the electrodes of the 16008B used.

FAQ 2010-07-02

在不使用 16453A 和 16454A 的情况下,E4991A 选件 002 是否可以测量电容率或导磁率?
否,使用 E4991A 选件 002 测量电容率或导磁率时,必须使用 16453A 或 16454A。

FAQ 2010-05-24

为什么总是在 16190B 空气管线中心导体的一侧刷上黑漆?
刷上黑漆标记是为了标明连接到测试端口的中心导体的方向。

FAQ 2010-05-24

有没有适用于扩展 E4991A 测试端口的选件或附件?
除了 E4991A-007 温度特征测试套件,不需要安装任何选件或附件来扩展 E4991A 的测试端口。

FAQ 2010-05-24

When fabricating a custom test fixture for the Keysight 4339B, what are the recommendations to extend the measurement and interlock cables?

FAQ 2010-05-11

如何订购 Keysight 42941A 阻抗探头的替换探针?
订购部件编号为 42941-60004 的是德产品

FAQ 2010-03-16

如何订购 4285A 选件 201、202 和选件 301 的操作指南?
4285A 选件 201/202 处理器接口和选件 301 扫描仪接口的操作指南列在 4285A 操作手册(序列号 04285-90010)结尾部分的附录中。

FAQ 2009-08-13

16047A 与 16047D 之间存在哪些差异?

FAQ 2009-08-13

How can I order 10 µF Standard Capacitor to retrofit the 16380C with Option 001?
The 16380V-001 Upgrade Kit for adding 10 µF capacitor is available.

FAQ 2009-07-07

Is there a 16060A-like transformer test fixture usable with the 4284A?
No transformer test fixture for the 4284A is available.

FAQ 2009-03-11

Can the 16092A Spring Clip Fixture be used with the 4287A?
Yes. Please refer to Test Fixtures/Accessories Quick Reference Matrix.

FAQ 2009-03-11

Is there a 16060A-like transformer test fixture usable with the E4980A?
No transformer test fixture for the E4980A is available.

FAQ 2009-03-11

What are the dimensions of the working standards supplied with the option 4287A-004?

FAQ 2009-03-11

16092A夹具是否可与4395A/4396B/4287A分析仪一起使用?

FAQ 2009-01-14

How can I replace the contact electrodes of the 16118A?
The contact electrodes of the 16118A cannot be replaced by user.

FAQ 2009-01-13

What are the differences between the 16048A and the 16048D?
The differences between the 16048A and 16048D are shown in the table below...

FAQ 2009-01-13

How can I get a 0603 size LOAD standard that can be used to perform LOAD correction using the 16196C and other SMD test fixtures?
Keysight part number 0699-6926 can be used as a LOAD standard. It is a 51-ohm chip resistor.

FAQ 2009-01-13

Can I use the 16048B with the 4285A for the cable extension?
Yes, the 16048B (Part Number 16048-60030) can be used with the 4285A. But, it is not easy to perform the cable correction using the 100-ohm resistor box (furnished with the 4285A).

FAQ 2009-01-13

What is the purpose of the grounding lead of the 16048D?
The grounding lead of the 16048D is used to interconnect this shielding conductor and the ground terminal on LCR meter's front panel.

FAQ 2009-01-13

当使用SMD夹具时,影响阻抗测量相关性的因素有哪些?

FAQ 2009-01-13

Isn't the current 16034E equipped with a dual-post stopper while previous ones had the stopper attached to the right side of Hcur connector?
The 16034E currently has no stopper because all impedance analyzers that required the stopper became obsolescence by 2001.

FAQ 2009-01-13

What compensation should I perform when I use the 16048B with the 4285A?
It is recommended to set the Cable Length function of the 4285A to "1 m" and perform open/short/load compensation at the DUT contact terminals of the test fixture connected to the tip of the 16048B.

FAQ 2009-01-13

以前 1 2 3 4 5 下一页