Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

retirer tout le raffinement

Par sujet

By Type of Content

Par catégorie de produit

151-175 of 418

Sort:
What options do the DSO3000-series oscilloscopes offer for saving data?
You can save data to internal oscilloscope memory or you can use the N2860A Scope Connect software to save data to your PC.

FAQ 2008-09-30

Can I automatically position the Y1 and Y2 cursors to the voltage values at X1 and X2?
Yes, using SCPI remote programming commands, follow these steps...

FAQ 2008-09-30

Is it possible to save a previous TDR measurement waveform and load as a comparison for my current TDR measurement?
It is possible to save a previous TDR measurement waveform and load it onto the oscilloscope as a comparison to the current measurement.

FAQ 2008-08-03

Is it possible to save multiple TDR traces and display them as waveforms on the oscilloscope for comparison to my current measurement?
It is possible to save multiple TDR traces as an internal format for future reference...

FAQ 2008-08-03

Can measurements be made on the saved waveforms?

FAQ 2008-08-03

Is it possible to upgrade my DSO6000 Series oscilloscope to a MSO model?
Yes, by purchasing one of these upgrade kits ...

FAQ 2008-08-01

Can a customer order MSO option with a 6000L scope?
Yes, customer can order N2914A MSO upgrade kit for DSO6014L (100MHz DSO) or N2915A MSO upgrade kit for DSO6054L/6104L.

FAQ 2008-08-01

How do I determine or adjust the sample rate of my 6000-series oscilloscope?
To determine the sample rate, press the Main/Delayed button. The scope will display the current sample rate in the lower left portion of the display.

FAQ 2008-07-31

Where are the NI instrument drivers for 6000 Series scopes?
National Instruments has developed two software drivers for our 6000 Series scopes (A and L Series). They both are downloadable from NI web sites below.

FAQ 2008-03-27

Do I need a J8130A in order to use the MSO6000 with option FRS?
Yes, the J8130A (VPT1000) is required in addition to order the option FRS on the MSO6000 in order to do FlexRay Measurements on the MSO6000. Without the VPT1000, there is no FlexRay functionality on the MSO6000. Keysight does provide an additional ...

FAQ 2008-02-19

If the J8130A must be purchased separately what are the required options to use it with the scope?
No extra options are required on the J8130A to run with the MSO6000. The plain J8130A product is sufficient. However, the J8130A has a few potential options that could be ordered if needed: -The option 001 allows the VPT1000 to be used as a Flex...

FAQ 2008-02-12

How many charges will the battery last through?
The battery should deliver >80% of initial capacity after 300+ charge/discharge cycles.

FAQ 2007-11-02

How many months/years is it expected to last?
Occasional battery users can use the battery ~10 years before replacement, while heavy users may need to replace within 2-3 years.

FAQ 2007-11-02

How much will it add to the weight of the scope?
12.35 Lbs without power adapter and 14 Lbs with power adapter

FAQ 2007-11-02

What is unique about Keysight’s battery powered oscilloscope?
Keysight’s 6000 Series with the battery option is the only battery powered mixed signal oscilloscope (MSO), highest performance 100MHz -500MHz battery powered oscilloscopes and only 1GHz battery powered oscilloscope available in the market.

FAQ 2007-11-02

If the battery dies and will not recharge, is it return to factory or service center for repair?
The oscilloscope battery is not user replaceable. You must return the oscilloscope to Keysight for battery replacement.

FAQ 2007-11-02

Is Keysight’s battery-powered scope safe to use?
Keysight’s battery powered 6000 Series scopes were designed and manufactured to meet strict safety measures and comply with international safety standards.

FAQ 2007-11-02

Is the battery option retrofitable to previously purchased oscilloscope?
No. The battery option for the 6000 Series is a factory-installed option which is not retrofitable to previously purchased oscilloscopes.

FAQ 2007-11-02

How do I maximize the battery life?
Avoid charging and discharging the battery repeatedly.

FAQ 2007-11-02

What comes with the 6000L Series oscilloscope?
The 6000L Series oscilloscope comes with the following items

FAQ 2007-11-02

What is the technology used in the battery powered 6000 Series?
Rechargeable lithium ion battery

FAQ 2007-11-02

How long does the charge last?
~2 hrs initially

FAQ 2007-11-02

What are the applications for battery-powered oscilloscope?
Battery-powered oscilloscopes are targeted for engineers and technicians in automotive testing, quality testing, industrial applications, power control circuit testing, In-vehicle, marine, and aerospace applications.

FAQ 2007-11-02

Is there a way to access online help for 6000L?
Yes. Press right mouse click on the specific softkey image.

FAQ 2007-11-02

Is it necessary to connect the ground post on the rear panel to earth ground?
If the circuit under test has voltages that exceed 30Vrms (or >42Vpk), the scope chassis needs to be connected to earth ground.

FAQ 2007-11-02

Previous 1 2 3 4 5 6 7 8 9 10 ... Next