Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

101-125 of 526

Sort:
How can I find accessories for a Keysight product?
For instrument-specific accessories (such as probes for an oscilloscope), first go to the product page and then see the related accessories. For general-purpose accessories (such as rf & microwave test accessories, carts, and racks), go to the ...

FAQ 2011-10-07

When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

Where can I find upgrade information of ENA?
Please refer to the ENA series service and support home page.

FAQ 2011-10-07

The ENA / ENA-L was infected with the virus. What should I do?
Remove the LAN cable and perform system recovery.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

What are the equations that relate Real and Imaginary data pairs to Log Magnitude, Polar, Phase, and Smith Chart formats?

FAQ 2011-10-07

Anti-Virus FAQ for ENA

FAQ 2011-10-07

ENA & PNA Series Network Analyzer Frequently-Asked Questions (FAQs)

FAQ 2011-10-07

Does the ENA contain parts with limited service life?
Yes.

FAQ 2011-10-07

Is there an error in the delay/thru definition for the 85039B F-Type Calibration Kit?
Yes.

FAQ 2011-10-07

After performing a calibration with a user defined calibration kit, all log magnitude data is displayed as -200 dB; why?

FAQ 2011-10-07

On the ENA and ENA-L, is there a SCPI command to query the active trace?
Yes.

FAQ 2011-10-07

Can I disable the front keys, keyboard, mouse and/or touch screen on the ENA / ENA-L?
Yes.

FAQ 2011-10-07

On the ENA / ENA-L, when recalling a state, the free running trigger condition is not being preserved. Why?
If the user selects either Save Type "State & Trace" or Save Type "All" then trace data is included as part of the state save.

FAQ 2011-10-07

What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

On the ENA / ENA-L, what is the meaning of "1.#QNB" or "1.#QNAN"?

FAQ 2011-10-07

Windows login process appears on my ENA every time after power up. Can I skip this?
Yes.

FAQ 2011-10-07

Can I modify the trace background color from black to white on the ENA?

FAQ 2011-10-07

Is it possible to control external instruments by the ENA/ENA-L?
Yes. It is possible to control external instruments by the ENA/ENA-L with built-in VBA programs.

FAQ 2011-10-07

On the ENA / ENA-L, it appears as though only the first channel is activated. Is this normal?
Yes

FAQ 2011-10-07

Are the adapters in the 85033E 30kHz to 9GHz calibration kit phase matched?
Yes.

FAQ 2011-10-07

My simulation software is failing to import Touchstone files with extensions *.s1, *.s2, etc. Is there a way to rectify this issue?

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

In limit line test, the marker value at that point is beyond the limit line. However, the Pass/Fail indicates a Pass condition. Why?

FAQ 2011-10-07

Previous 1 2 3 4 5 6 7 8 9 10 ... Next