这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

101-125 / 526

排序:
When I save a Touchstone file with the ENA / ENA-L, which calculation will be reflected in the Touchstone file?
All calculations are reflected in the Touchstone file except for the mixed-mode conversion.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

What are the benefits of the built-in VBA?

FAQ 2011-10-07

ENA 代码是否兼容 8753?
否,但代码转换辅助编辑器可帮助进行代码转换。

FAQ 2011-10-07

有没有Keysight VEE示例程序概括说明如何使用SRQ通过程序来检测ECal校准过程是否完成?
有。

FAQ 2011-10-07

在Keysight ENA和ENA-L系列矢量网络分析仪上,如何确定硬盘版本?

FAQ 2011-10-07

On the ENA / ENA-L, when recalling a state, the free running trigger condition is not being preserved. Why?
If the user selects either Save Type "State & Trace" or Save Type "All" then trace data is included as part of the state save.

FAQ 2011-10-07

能否改变ENA上功能键菜单的字体大小?
能。可通过以下步骤改变功能键菜单字体的大小…

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

存储屏幕图像时,如何关闭ENA/ENA-L上的功能键?

FAQ 2011-10-07

在什么地方可以找到 ENA 的升级信息?
请参见 ENA 系列服务和支持主页。

FAQ 2011-10-07

ENA 和 ENA-L 感染了病毒,应该怎么办?
客户应该在第一时间除去网络线并执行系统恢复。

FAQ 2011-10-07

是否可以将ENA系列网络分析仪的路径背景色由黑改为白?

FAQ 2011-10-07

ENA & PNA Series Network Analyzer Frequently-Asked Questions (FAQs)

FAQ 2011-10-07

Windows login process appears on my ENA every time after power up. Can I skip this?
Yes.

FAQ 2011-10-07

关于电缆测试设备,用户应该使用TDR、网络分析仪,还是两者皆用?

FAQ 2011-10-07

在 ENA 和 ENA-L 上是否有查询活动通道的 SCPI 命令?

FAQ 2011-10-07

Is it possible to control external instruments by the ENA/ENA-L?
Yes. It is possible to control external instruments by the ENA/ENA-L with built-in VBA programs.

FAQ 2011-10-07

ENA/ENA-L的前面板按键,键盘,鼠标和触摸屏可以锁住吗?
是的,可以。

FAQ 2011-10-07

使用用户定义的校准套件执行校准后,所有记录幅值会显示为-200dB,这是什么原因?

FAQ 2011-10-07

我该如何配置Keysight IO程序库套件14,以便通过局域网与ENA进行通信?

FAQ 2011-10-07

Anti-Virus FAQ for ENA

FAQ 2011-10-07

What are the equations that relate Real and Imaginary data pairs to Log Magnitude, Polar, Phase, and Smith Chart formats?

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页