Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

126-150 of 1734

Sort:
Can I remotely query the 86100D DCA-X to determine which user interface is running?
Yes. Issue the query :SYSTem:FCONfig? If the response is "Legacy" then the legacy UI is in use. If the response is "Compatible" or "Standard" then the FlexDCA interface is in use.

FAQ 2012-12-12

What is the difference between E2731A & E2731B or E2730A & E2730B tuners for 89600S vector signal analyzer?
There are no visible differences, but there is a performance difference relating to the local oscillators.

FAQ 2012-12-10

What is SCANSTA112 device?
The SCANSTA112 device is a 7-port multidrop IEEE 1149.1 (JTAG) multiplexer design to connect boundary scan chains into a single chain as well as the ability to remove a board from the system and retain test access to the remaining chains.

FAQ 2012-12-01

What are the failures that boundary scan test can detect?
Boundary Scan test will be able to diagnose the following failures:

FAQ 2012-12-01

Why are some of the features shown in the Framescope user manual not available in software version 7.0.5?
Users might encounter different features when using Framescope software version 7.0.5 versus what is stated in the documentation.

FAQ 2012-11-28

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

What are the differences between the 6632A/33A/34A and 6632B/33B/34B?
Some functions such as accuracy and programming commands are enhanced in “B” version.

FAQ 2012-11-05

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

Will the external mixer Option EXM support the 11974 Series preselected mixers?
There are no plans to support the 11974 Series preselected mixers with the N9030A PXA.

FAQ 2012-10-25

How can I order replacement protective caps for waveguide flanges?

FAQ 2012-10-23

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

What external mixers will work with my PXA/mmW EXA and how do I order them?
Currently, the N9030A PXA/mmW EXA with Option EXM will work with either the 11970 Series (with the exception of the 11970K) or ) or external mixers from other vendors such a OML Inc. mixers.

FAQ 2012-10-17

Which Keysight oscilloscopes have a 10 MHz reference input/output?
6000 Series, 6000L Series, 7000A Series, 7000B Series, 9000 Series, 54850 Series (Output only), 80000A Series, 80000B Series, 90000A Series and 90000 X-Series

FAQ 2012-10-17

FrameScope Pro Download

FAQ 2012-10-16

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

IO Libraries Suite: Can I use VXI on a 64-bit OS?
IO Libraries Suite 16.1 (or later) supports VXI (E8491A/B and E1406A) on 64-bit Vista, 7, Server 2008 R2...

FAQ 2012-10-10

IO Libraries Suite: How do I obtain a license for the Keysight IO Libraries Suite?
Keysight now allows you to use the IO Libraries Suite, whether or not you have Keysight equipment...

FAQ 2012-10-10

IO Libraries Suite: Can a customer shipped the current version of the Keysight IO Libraries Suite use a previous version?
Yes.

FAQ 2012-10-10

IO Libraries Suite: What is IO Monitor?
IO Monitor is a utility that traces the I/O calls of the Keysight VISA, VISA COM and SICL I/O libraries.

FAQ 2012-10-10

What is the CAPTURE State?
During the CAPTURE state, data or instruction bits are loaded in parallel into data or instruction registers. The CAPTURE-DR (Data Register) loads data bits into the specified data register. CAPTURE-IR (Instruction Register) loads instruction bits into the Instruction Register.

FAQ 2012-10-01

Why do I need to hold the state of certain pins/nodes?
Non-boundary scan devices such as DDR or flash memories need to hold one or more nodes (chip select/enable) to fixed states during boundary scan testing, so that the device is disabled during boundary scan testing and its output pins (i.e. data) are not activated, as otherwise, it will cause unstable tests or damage to the circuitry. Boundary scan “hold states” are node/device pins on a board that are held to a logic of 1 or 0 by a boundary scan driver on the node, when the boundary scan device driver/output pin is in EXTEST.

FAQ 2012-10-01

All IntuiLink Tools for Keysight Oscilloscopes
Supported Models: Infiniium Series, 1000 Series, 2000 X-Series, 3000 X-Series, 5000 Series, 6000 Series, 7000 Series, and 54600 Series Oscilloscopes

FAQ 2012-09-26

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

How can I de-embed a test fixture using the 86100C/D Digital Communications Analyzer?
N1010A software with InfiniiSIM-DCA option provides the capability to de-embed and embed fixtures, cables, probes, and other circuit elements.

FAQ 2012-09-25

Previous 1 2 3 4 5 6 7 8 9 10 ... Next