您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

76-100 / 165

排序:
Passive Filter Synthesis
Learn how to quickly design LPF, BPF, HPF and Bandstop filters from a complete selection of response shapes such as Chebyshev, Butterworth, Cauer, Bessel or user-defined G-value tables. Automatically calculate LC component values for single-ended or balanced differential topologies for fast realization with passive filter synthesis. Includes singly terminated topologies for diplexer and multiplexer designs.

基本展示 2015-08-15

Equalization Network Synthesis
Learn how to quickly design active and passive equalization networks to correct for group delay and phase distortions in your RF systems or circuits such as filters and amplifiers defined by measured S-parameters or equivalent circuits. Automatically calculate and optimize component values of analog equalization networks with equalization network synthesis.

基本展示 2015-08-15

Splitter, Coupler, Balun and Attenuation Synthesis
Learn about RF/microwave signal control using splitters, combiners, couplers, baluns and attenuators. Then quickly design from 27 different popular topologies such as Wilkinson splitter, Lange Coupler and 90 degree branch line including generation of their distributed layouts on microstrips using signal control synthesis.

基本展示 2015-08-15

Phase Locked Loop PLL Synthesis
Designing phase locked loops (PLL) for frequency synthesizers or frequency/phase modulator/demodulator can be a daunting task because of the multiple interactions of the PLL components such as reference source, loop filter, phase-frequency-detector, divider and VCO. PLL synthesis interactively guides the designer in selecting the appropriate specs for these components in order to achieve the desired balance of loop stability, phase noise and lock time.

基本展示 2015-08-15

Oscillator Synthesis
Learn the foundations of practical RF oscillation design in understanding the interaction of loop gain, zero phase crossing, phase slope and resonator characteristics on oscillator performance and transient startup. Then know how to select from 19 types of oscillator topologies and design them quickly with automatic calculation and optimization of component values through oscillator circuit synthesis.

基本展示 2015-08-15

RF Mixer Synthesis
Learn about RF mixer characteristics and how to select from 11 different passive and active topologies including single ended, balanced, double-balanced and Gilbert Cell for achieving the required frequency translation conversion gain and LO-RF-IF isolation. Then design them quickly with automatic calculation of component values through mixer circuit synthesis.

基本展示 2015-08-15

IMS 2015 Demos from Keysight EEsof EDA
YouTube video playlist containing International Microwave Symposium (IMS) 2015 demo videos from Keysight EEsof EDA MicroApps.

基本展示 2015-06-19

How to Match RF Impedance Effectively By Optimally Selecting SMT Devices
This video demonstrates a very effective RF impedance matching methodology with SMT devices that helps RF engineers save time and cost. With this methodology, RF engineers can start to match the design with a list of good combinations of SMT devices which satisfies the target impedance and loss specifications instead of trying out unlimited possibilities at the workbench. This methodology should work very well with typical wireless or mobile product designs such as smart phones.

使用說明影片 2015-06-11

How to Design for Power Integrity: Finding Power Delivery Noise Problems
This video provides an understanding of how the voltage regulator module (VRM) interacts with the printed circuit board planes and decoupling capacitors within a power distribution network (PDN). A well designed PDN provides optimum system performance while a poorly matched designed PDN can result in poor system performance. In the extreme case, rogue waves can occur within the PDN generating much higher voltage noise levels than expected, potentially interfering with system performance or resulting in permanent damage. Recommendations for keeping the impedance flat are also provided.

使用說明影片 2015-06-05

Microwave Journal - Keysight 5G Design and Verification
Microwave Journal video: 5G Applications Development Engineer Greg Jue demonstrates one of Keysight's latest innovations.

基本展示 2015-06-02

Microwave Journal - Keysight Interview with Todd Cutler
Microwave Journal Editor Pat Hindle interviews Todd Cutler, General Manager of Keysight EEsof EDA.

基本展示 2015-05-31

How to Design an RF Power Amplifier: Class J
This short video will provide an introduction to Class J Power Amplifiers and demonstrate a superior, time saving methodology to design and practically realize a Class J RF power amplifier. First,a theoretical approach will be used to design an ideal circuit from first principles and then circuit design tools will be utilized to synthesize a more realistic circuit topology from the ideal case. The design process will be illustrated using a commercially available GaN MMIC device from Qorvo.

使用說明影片 2015-05-07

How to Understand 5G: Waveforms
This video will provide you with good guidance for understanding what kinds of new waveforms are being researched for the next generation standard. The example with end-to-end link level simulation will demonstrate waveform quality issues of a multi-carrier system and the nonlinearity from the RF chain.

使用說明影片 2015-05-01

Using SystemVue to generate IBIS AMI models
Use SystemVue to design your next gigabit SerDes link with great physical layer insights, and then quickly generate IBIS AMI models to act as a "transportable datasheet" for your design.

基本展示 2015-04-23

Keysight EEsof EDA "How To Design Power Amplifier" Videos
A collection of "How to Design Power Amplifier" Videos from Keysight EEsof EDA.

使用說明影片 2015-04-22

Discovering SystemVue - MATLAB Script Modeling
Keysight SystemVue now includes MATLAB Script, an equation and modeling engine from MathWorks. This product tutorial shows communications system designers how to create and debug MATLAB models from inside the SystemVue user interface.

基本展示 2015-04-15

Keysight WaferPro Express
The Keysight WaferPro Express software performs automated wafer-level measurements of semiconductor devices such as transistors and circuit components. It provides turnkey drivers and test routines for a variety of instruments and wafer probers. Its user interface makes it easy to setup and run complex wafer-level test plans, while powerful customization capabilities are enabled by the new Python programming environment.

產品導覽 2015-03-24

5G 通道探量
這個影片討論了是德科技的 5G 毫米波 MIMO 通道探量解決方案。5G 的目標是實現隨時隨地的通訊,並將資料速率大幅提升到 gigabyte 等級。為此,我們需使用新技術,例如 massive MIMO 和 5G 毫米波寬頻解決方案。5G 的目標是實現隨時隨地的通訊,並將資料速率大幅提升到 gigabyte 等級。為此,我們需使用新技術,例如 massive MIMO 和 5G 毫米波寬頻解決方案。

基本展示 2015-03-19

How to Design an RF Power Amplifier: Class E
This video provides an introduction to Class E Power Amplifiers and demonstrates a superior, time saving methodology to design and practically realize a Class E RF power amplifier using first principles to build an ideal circuit and then utilizing circuit design tools to synthesize a more realistic circuit topology from the ideal case.

使用說明影片 2015-03-11

How to Do Fixture De-embedding to Match Signal Integrity Simulations to Measurements
This video provides a quick overview of how fixture de-embedding from measurements, or embedding into simulations is a critical step for matching simulations to measurements for physical layer Tx to Rx channels.

使用說明影片 2015-03-10

Keysight 5G signal generation and analysis demonstration at Mobile World Congress
Keysight demonstrates candidate 5G FBMC waveform co-existence with 4G LTE, and up to 2GHz wideband FBMC signal generation and analysis using SystemVue W1906 5G library, N7608B Signal Studio for custom modulation, and 89600 VSA software applications with Keysight wideband test equipment.

基本展示 2015-03-09

Keysight 5G Millimeter-Wave Channel Sounding demonstration at Mobile World Congress
Keysight demonstrates a multi-channel Channel Sounding system at milimeter-wave frequencies, to enable 5G research and system validation

基本展示 2015-03-09

How to Predict Package and Bondwire Effects on Your RF-Module Designs
This short video shows how to predict package, board, and bond wire effects on your RF-module designs which subsequently enables you to fix the design prior going to fabrication. The video demonstrates the process of building modules that comprise different technologies and performing EM simulation on them.

使用說明影片 2015-02-19

How to Use Envelope Tracking to Improve Power Amplifier Efficiency
This video introduces basic concepts regarding applying envelope tracking to improve power amplifier efficiency.

使用說明影片 2015-02-10

How to Make Accurate, Automated RF Wafer-level Measurements
The video introduces automation as a way to increase productivity and efficiency. Keysight WaferPro Express measurement software is used to illustrate the various steps in combination with Cascade Microtech Velox software for prober control and Cascade WinCalXE software for automated calibration.

使用說明影片 2015-01-27

上一個 1 2 3 4 5 6 7 下一頁