您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

51-75 / 107

排序:
Keysight press release on introduction of new arbitrary waveform generator M8196A, September 2015
Keysight press release on introduction of new arbitrary waveform generator M8196A, September 2015

新聞資料 2015-09-17

IVI Driver Reference
Keysight's IVI drivers simplify the creation and maintenance of instrument control applications in a variety of development environments.

輔助說明檔 2015-07-28

ZIP ZIP 1.33 MB
LabVIEW G Programming Information
This help file contains LabVIEW G programming guidelines and reference information for the M9330A Series Arbitrary Waveform Generator.

輔助說明檔 2015-07-28

ZIP ZIP 1.24 MB
Generating PAM-4 Signals using an M8195A AWG
Learn about using the M8195A Arbitrary Waveform Generator in conjunction with a 33 GHz real time scope to generate PAM-4 signals. As well as how to calibrate the set up for optimal frequency response. And some capabilities of the M8195A in terms of modifying and changing the characteristics of the PAM-4 signal.

基本展示 2015-07-08

Fundamentals of Arbitrary Waveform Generation, AWG Primer - Reference Guide
This primer discusses characteristics and fundamentals of arbitrary waveform generation and the different implementations available in the market. It also shows examples how to generate digital, multi-level and PAM4 signals, wireless and modulated waveforms, multi-carrier as well as coherent optical signals.

參考指南 2015-06-01

M8195A 任意波形產生器 - 操作指南(適用於 rev. 1 硬體的舊版本)
M8195A 65 GSa/s 任意波形產生器結合業界最高的速度、頻寬和通道密度。 它可在高達 32 Gbaud 的速率下提供靈活的信號產生能力。利用乾淨和失真信號對裝置進行極限應力測試。

使用手冊 2015-05-01

M8195A Arbitrary Waveform Generator OFC Video 2015
An overview of what an AWG is and what the advantages of using an AWG for optical applications are; which applications are supported by an AWG in the optical space and what the advantages of the Keysight M8195A over other AWG’s in the market are.

基本展示 2015-04-20

MIPI M-PHY, D-PHY and C-PHY Receiver Testing- Recorded webcast
MIPI M-PHY, D-PHY and C-PHY Receiver Testing- Recorded webcast

基本展示 2014-11-03

AWG article - MWJ product feature
AWG article - MWJ product feature

專文 2014-10-14

M8195A 任意波形產生器–入門指南
M8195A 65 GSa/s 任意波形產生器結合業界最高的速度、頻寬和通道密度,它可在高達 32 Gbaud 的速率下提供靈活的信號產生能力,利用乾淨和失真信號對裝置進行極限應力測試。

快速入門指南 2014-10-01

M8195A 65GSa/s AWG – Press Release
Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator

新聞資料 2014-09-10

Keysight M8195A AWG - The Digital and Arbitrary Signal Generator
Keysight M8195A AWG - The digital and arbitrary signal generator with the highest combination of speed, bandwidth and channel density The M8195A AWG is a high speed AWG with up to 65 GSa/s sample rate and 20 GHz bandwidth on up to 4 channels per module.

基本展示 2014-09-08

M8195A 65 GSa/s 任意波形產生器 - 產品規格書
Keysight M8195A 為新型任意波形產生器,具有業界最高的取樣率、頻寬和通道密度。可以高達 32 Gbaud 的速率產生信號。

產品型錄 2014-09-08

Keysight M8195A AWG within the Mobile & Network Ecosystem
As devices and interfaces become faster and more complex, the M8195A AWG gives you the versatility to create the signals you need for digital applications, optical and electrical communication, advanced research, wideband radar and satcom.

基本展示 2014-09-08

Microwave Frequency Up-Converters Extend Signal Simulation to 40 GHz – Synopsis
Microwave frequency up-converters extend signal simulation to 40 GHz from Synopsis and Keysight

解決方案簡介 2014-08-04

Using Flexible Digital Modulation Testing for Satellite Regenerative Payloads - Application Note
This application note focuses on solutions for the issues that create risks in the integration of mixed-signal systems with a mix of software and hardware tools. Examples focus on measurements of error vector magnitude (EVM), which is a key figure of merit for modulated signals implemented in either analog or digital form.

應用手冊 2014-08-01

Wideband Digital Pre-Distortion with Keysight SystemVue & PXI Modular Instrument - Application Note
Digital Pre-Distortion (DPD) is essential for wideband communications systems based on LTE-Advanced and 802.11ac. Overcome DPD challenges with trusted commercial measurement and modeling tools.

應用手冊 2014-08-01

Satellite Test Solution – AAI
Satellite Payload and Panel Test Solution from AAI and Keysight Technologies

解決方案簡介 2014-04-09

A new approach for multi-emitter test signal generation – Article
A new capture and playback approach generates multi-emitter test signals using a combination of COTS test equipment and simulation software.

專文 2013-11-15

Enhancing microwave spectroscopy in astrophysics applications – Article
An arbitrary waveform generator is the key element in this faster and more accurate method.

專文 2013-11-15

Meeting satellite testing challenges - Article
Satellites are now a critical part of the infrastructure supporting the incredible growth in demand for broadband data.

專文 2013-11-13

Understanding 802.11ad Physical Layer and Measurement Challenges Tutorial
View this 6-part recorded tutorial presented by Keysight experts for an overview of standards and market trends followed by an in-depth description of the physical-layer construction.

使用手冊 2013-09-20

Press Releases for M8190A

新聞資料 2013-09-06

Press Release for M8192A
Infinite Playtime and Multichannel Support introduced for Arbitrary Waveform Generator

新聞資料 2013-09-05

M8190A Arbitrary Waveform Generator - Videos
M8190A Arbitrary Waveform Generator - Videos

基本展示 2013-09-04

上一個 1 2 3 4 5 下一頁