기술 지원
151-175 / 3285
Addressing the Challenges of High-Speed Digital I/O for Aerospace Defense – Application Note
This application note will also discuss test challenges and commercial test solutions for fiber digital I/O technologies to help mitigate risk in upgrading to fiber-based technologies.
어플리케이션 노트 2017-12-01 |
|
Measuring Battery Life on Battery-Powered Medical Devices
Understand the power consumption patterns and battery life requirements of electronic consumer medical devices designed to meet the demanding needs of the end users.
어플리케이션 노트 2017-12-01 |
![]() |
IoT – With Great Power Comes Great Challenges
Addresses the rising challenges for IoT device designers and developers at component, circuit and system levels.
어플리케이션 노트 2017-12-01 |
![]() |
CAN FD Eye-Diagram Mask Testing
Learn more about eye-diagram testing for higher speed buses such as the CAN FD serial bus.
어플리케이션 노트 2017-12-01 |
![]() |
Secondary Radar Transponder Testing Using the 8990B Peak Power Analyzer - Application Note
Learn how 8990B PPA can be used to execute periodic maintenance and calibration of aircraft transponder or transponder test set. 8990B PPA is used to analyze and measure interrogation and reply pulses.
어플리케이션 노트 2017-12-01 |
![]() |
Best Practices For Making The Most Accurate Radar Pulse Measurements - Application Note
Learn how to make the most accurate radar pulse measurements. This article also covers real-world scenarios that demonstrate how to carry out these tips with Keysight power meters and sensors.
어플리케이션 노트 2017-12-01 |
![]() |
Making Conducted and Radiated Emissions Measurements - Application Note
This application note provides an overview of radiated and conducted emissions measurements as well as a methodology for EMI precompliance testing.
어플리케이션 노트 2017-12-01 |
![]() |
DDR Probing for Physical Layer and Functional Testing - Application Note
Probing is the key to accessing signals and validating your designs. Although you may normally probe at signal vias or designed-in probe points, for DDR these do not always provide good signal integrity.
어플리케이션 노트 2017-12-01 |
![]() |
Overcoming the Challenges in Satellite Testing and Interference Detection - Application Note
With a streamlined multi-touch UI, wider bandwidth and application software, the Keysight PXA offers the tools you need to design, test and deliver your next breakthrough in satellite communications.
어플리케이션 노트 2017-12-01 |
![]() |
Understanding the Right Metrics to use when Evaluating Oscilloscope Quality - Application Note
For scopes with bandwidth in the GHz range, a quality metric involves characterizing the analog-to-digital converter (ADC) using effective number of bits (ENOB). How important is ENOB?
어플리케이션 노트 2017-12-01 |
|
Time-Saving Features in Economy Oscilloscopes Streamline Test - Application Note
Features like integrated function generators, large displays, fast update rates and mixed signal capabilities are now available in oscilloscopes to save valuable time in the design and debug process.
어플리케이션 노트 2017-12-01 |
![]() |
Capturing Events of Long Duration or High Data Volume
This application note describes four system configurations on Keysight digitizers that support data streaming, the potential bottlenecks, and possible solutions to the bottlenecks.
어플리케이션 노트 2017-12-01 |
|
Measuring Polarization Dependent Loss of Passive Optical Components - Application Note
A new document on the methods of characterizing passive optical components.
어플리케이션 노트 2017-12-01 |
![]() |
Gap-free Recording and Analysis of Elusive, Intermittent Signals Made Simple - Application Brief
A turnkey RF streaming solution from Keysight Technologies, Inc. and X-COM Systems simplifies recording and analysis of elusive and intermittent signals, enabling up to 255 MHz analysis BW to 50 GHz.
어플리케이션 노트 2017-12-01 |
|
에너지 효율이 높은 입력 전압 통신 장비 개발을 위한 전력 소스(영어)
통신 장비 개발자는 고전압 배전을 이용하는 네트워크 설비의 새로운 통신 장비를 개발하기 위한 테스트 시스템의 전원을 선택할 때 몇 가지 과제에 직면합니다.
어플리케이션 노트 2017-11-30 |
|
How to Easily Create an Arbitrary Waveform Without Programming - Application Note
Creating arbitrary waveforms on a modern function generator or arbitrary waveform generator (AWG) is not as difficult as you might think. Many engineers try to avoid creating arbitrary waveforms (arbs) at all costs. When they hear the word “arb“, they picture the tedious process of learning how to use some type of waveform software or, worse yet, having to write a program to generate a waveform and then remotely connecting to your AWG to upload the arb. With modern AWGs, creating an arbitrary waveform no longer has to be looked upon with doom and gloom.
어플리케이션 노트 2017-11-27 |
![]() |
FFT and Pulsed RF Measurements with 3000T X-Series Oscilloscopes - Application Note
Explore how FFT math functions and spectral views on a 3000T X-Series oscilloscope help to bring digital and RF designs to market.
어플리케이션 노트 2017-11-23 |
|
8 Hints for Better Scope Probings - Application Note
In this application note, you will find eight useful hints for selecting the right probe for your application and for making your oscilloscope probing better.
어플리케이션 노트 2017-11-23 |
|
Using AFM and Nanoindentation Techniques for Comprehensive Nanomechanical Analysis of Materials
Comprehensive nanomechanical property studies of several polymer samples and metallic alloy of Bi/Sn are performed on both Keysight 9500 AFM and G200 Nanoindenter with good consistency in results.
어플리케이션 노트 2017-11-21 |
![]() |
Data Logging and Digitizing with a Digital Multimeter (DMM)—It’s about time! - Application Note
Now -- data logging and digitizing optimized in a DMM for optimized front panel operation rathern than remote programming and data transfer.
어플리케이션 노트 2017-11-16 |
![]() |
5G NR 디바이스 및 시스템 개발을 위한 OTA 테스트-백서
This document discusses the challenges of over-the-air (OTA) testing and the associated test methods of millimeter-wave devices, including phased array technology, millimeter wave beamforming and beamsteering.
어플리케이션 노트 2017-11-15 |
![]() |
OTA Test for Millimeter-Wave 5G NR Devices and Systems - White Paper
This document discusses the challenges of over-the-air (OTA) testing and the associated test methods of millimeter-wave devices, including phased array technology, millimeter wave beamforming and beamsteering.
어플리케이션 노트 2017-11-15 |
![]() |
Preserve Measurement Integrity of Your Test Equipment
Your peace of mind with maximum return on your investment
어플리케이션 노트 2017-11-13 |
|
Six Reasons Your New IoT Device Will Fail
Perform higher level tests to ensure your device will be able to function in today's crowded radio bands.
어플리케이션 노트 2017-11-13 |
![]() |
새로운 IoT 기기가 실패하는 6가지 이유 - 어플리케이션 노트(영어)
새로운 IoT 무선 기기를 아무리 신중하게 테스트했다 하더라도, 랩에서는 완벽하게 작동하지만 실제 환경에서는 실패할 수 있습니다. 그렇다면 그 원인은 무엇일까요?
어플리케이션 노트 2017-11-13 |
![]() |