这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-23 / 23

排序:
Why is the segmented memory acquisition mode useful and which Infiniium oscilloscopes support it?
Segmented memory mode offers more efficient acquisition memory usage for storing waveforms with events of interest that are separated by long periods of time. All currently shipping Infiniiums and many older units support segmented memory.

FAQ 2013-09-18

InfiniiVision 示波器上的 Auto(自动)和 Normal(常规)触发模式有什么区别?
在自动触发模式中,即便没有满足指定条件,触发器也将进行触发。在常规触发模式中,只有在满足指定条件时,触发器才会进行触发。

FAQ 2012-10-30

我能否手动设置 InfiniiVision 示波器的采样率?
虽然在任何 InfiniiVision 示波器上都不能直接设置采样率,但是可通过调节示波器的时间/格设置,间接地设置采样率。

FAQ 2012-10-30

哪些型号的是德示波器具有 10 MHz 参考输入/输出?
6000 系列,6000L 系列,7000A 系列,7000B 系列,9000 系列,54850 系列,(只有输出),80000A 系列,80000B 系列,90000A 系列,90000 X 系列

FAQ 2012-10-30

如何使用 86100C/D 数字通信分析仪去嵌入测试夹具?
配有 InfiniiSIM-DCA 选件的 N1010A 软件能够嵌入和去嵌入夹具、电缆、探头及其它电路元件。

FAQ 2012-09-25

54600系列或6000系列示波器可以使用通道3 和4来支持XY模式或数学函数吗?
这些示波器能够处理大量数学函数,例如在任意模拟通道上,甚至在其他数学函数上进行FFT、积分和微分运算。

FAQ 2011-06-22

如何从Infiniium示波器中获得最大可用存储器深度?
各种型号的Infiniium示波器可以提供每通道32K至128M点存储器的存储器深度。以下指南告诉您如何从特定的示波器中获得最大可用存储器。

FAQ 2011-06-07

如何将 Infiniium 示波器设置为 XY 模式?
所有型号的 Infiniium 示波器都有一个名为“versus”的数学函数,该函数可绘制出一个通道或函数与另一个通道或函数的关系图。

FAQ 2011-06-06

使用是德示波器的TV触发模式时,能否单独在触发偶数场或奇数场?
能。当前所有拥有TV触发功能的是德示波器均可单独进行偶数场触发或奇数场触发。

FAQ 2011-04-20

Are the input channels on the U1602B and U1604B Handheld Oscilloscopes isolated?
No, both scope channels (channel 1 and channel 2) on the U1602B and U1604B Handheld Oscilloscopes are not isolated.

FAQ 2011-03-31

For the InfiniiMax probes, what effect does the "Signal being probed" setting have? Why do I have to specify single-ended or differential?
Infiniium scopes and InfiniiMax differential probe amplifiers have a unique method of applying DC offset which considers whether the signal being probed is single-ended or differential...

FAQ 2010-10-06

How do I extract the 32Mpts from U270xA?
One way of “viewing” the full memory waveform is using the zoom function (that the red arrow...

FAQ 2010-09-14

Why does the pulse shape of my scope probe compensation look different from the pulse shape shown…
The compensation signal (square wave) that you see is different from the pulse shape shown in the U1602A/U1604A's user’s manual because….

FAQ 2010-08-09

How do I convert *.svw file to *.csv file in PC Link for U160xA/B?
1) From within PC Link, click on the "Load SVW" icon on the tool bar...

FAQ 2010-07-18

My InfiniiMax probe fails calibration or does not accurately pick up the cal signal when I use the E2655A test fixture. What could be wrong?
The first step in troubleshooting a failed probe calibration should be to compare the actual signal and the probed signal. If the probed signal does not track the actual signal well, it is most likely due to a poor connection.

FAQ 2010-03-09

Keysight Infiniium Oscilloscopes: Programming the Oscilloscope
Use the example programs and programming manual available for download from this web site.

FAQ 2009-12-11

How can I use a Keysight oscilloscope as a basic I-V curve tracer?
You can use the ocsilloscope's XY mode to plot I-V characteristics...

FAQ 2008-10-13

Can I automatically position the Y1 and Y2 cursors to the voltage values at X1 and X2?
Yes, using SCPI remote programming commands, follow these steps...

FAQ 2008-09-30

Why do I see more noise on my oscilloscope when a probe is connected?
When a probe is connected, the scope changes its attenuation setting so that it correctly displays the voltage coming from the probe.

FAQ 2006-12-04

Keysight Infiniium Oscilloscopes: Can You Trigger One Keysight Infiniium Oscilloscope From Another?

FAQ 2003-08-01

Keysight Infiniium Oscilloscopes: What Trigger Modes Does the Instrument Have?

FAQ 2003-08-01

Keysight Infiniium Oscilloscopes: Will Keysight Infiniium Scopes Trigger on HDTV Signals?

FAQ 2003-08-01

1653xA: Can I Do High Frequency Rejection to Filter a Signal Captured by the 16534A?

FAQ 2002-06-27