这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-13 / 13

排序:
What parts and accessories are available for my 10400A-series probe?

FAQ 2013-11-15

What are the rack mount kit part numbers for the 86100 DCA?
Rack mount kits for 86100 DCA are available to purchase as stand-alone parts.

FAQ 2012-12-20

How do I order the Infiniium oscilloscope hard drive replacement kit?
For Infiniium oscilloscopes with the Windows® XP operating system, the part number depends on the oscilloscope model number ...

FAQ 2012-11-13

如何为是德产品找到附件?
对于特定仪器附件(例如,用于示波器的探头),您首先应该访问产品页面,然后再查阅相关附件。 对于通用附件(例如,射频和微波测试)

FAQ 2011-10-07

我是否可以将电探头(1130A/31A/32A/34A)与86100 DCA 模块一同使用?
可以,N1022A探头适配器允许Infiniimax探头(1130A/31A/32A/34A)与86100 DCA模块一同使用。

FAQ 2011-07-23

What replacement parts and accessories are available for the 113xA-series InfiniiMax probes?
The best place to find this information is in the most recent revision of the InfiniiMax Active Probes User´s Quick Start Guide.

FAQ 2010-06-07

How to measure temperature with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
The humidity can be measured with U1586A Temperature Adaptor connected to the U1602A/U1604A handheld Oscilloscope

FAQ 2009-09-29

How to measure current with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
The current can be measured with connect a current adaptor (current probe) to the U1602A/U1604A handheld Oscilloscope...

FAQ 2009-06-10

If the J8130A must be purchased separately what are the required options to use it with the scope?
No extra options are required on the J8130A to run with the MSO6000. The plain J8130A product is sufficient. However, the J8130A has a few potential options that could be ordered if needed: -The option 001 allows the VPT1000 to be used as a Flex...

FAQ 2008-02-12

What digital probe cables and accessories are available for Keysight mixed-signal oscilloscopes (MSOs)?
The digital probe kit for all Keysight 6000-series and 54620/40-series MSOs is P/N 54620-61801. The digital probe kit for all 8000-series and 54830-series MSOs is P/N 54826-68701.

FAQ 2007-08-10

如何在新版本中打开旧的是德逻辑分析仪应用文件?
如果您有2.5版本之前的是德逻辑分析仪应用软件文件(文件扩展名.ala),并且无法在当前的是德逻辑分析仪应用软件中打开它们,您必须先在2.5版本的软件中打开这些文件,然后就能在最新版本的软件中打开它们

FAQ 2007-06-04

我的逻辑分析仪可以使用什么探头?
是德提供以下四种基本类型的逻辑分析仪探头...

FAQ 2007-06-01

What types of removable disk drives do Infiniium scopes have?
Since their introduction in 1997, Infiniium scopes have offered several removable disk formats.

FAQ 2005-02-14