您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-25 / 414

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

Are there 3D models of the Infiniium UXR-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2019-02-19

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

Is there a 3D model of the P9241A USB oscilloscopes?
Yes, see the IGES, Step, and PKG format file downloads.

FAQ 2018-09-21

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-07-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

XY Display Mode Example
The XY time mode converts the oscilloscope from a volts-versus-time display to a volts-versus-volts display using two input channels.

FAQ 2017-02-24

正在尋找效能優異的經濟型示波器嗎?
專業級品質、低成本示波器。Keysight 1000 X 系列示波器證明經濟型示波器也能具有高品質。

FAQ 2017-02-07

Is there a 3D model of the Infiniium V-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2017-01-25

Infiniium Oscilloscope HDD/SDD in Secure Environments
This FAQ talks about how to deal with Infiniium oscilloscope HDD/SDD in secure environments if you need to send oscilloscopes in for calibration.

FAQ 2016-09-26

Is there a 3D model of the InfiniiVision 6000L Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2016-07-18

Which printers are supported by the handheld oscilloscopes?
Keysight handheld oscilloscopes support PCL6, 5e,5c and Postscript level 3 emulation printer command languages.

FAQ 2015-11-09

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Does the 86100D DCA-X Support Windows 7?
Yes. Existing mainframes my be upgraded by ordering 86100DU-WN7 from your local contact center. All the new 86100Ds ship with Windows 7 installed.

FAQ 2014-09-25

Is there a 3D model of the InfiniiVision 6000 X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2014-04-29

Will the 86100C DCA-J be updated to support Windows 7?
No, the 86100C platform and software will not support Windows 7.

FAQ 2014-04-18

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Does PC link 2.51 support Windows 7, 64 bits?
No

FAQ 2014-04-17

What are the remote control commands to switch between FlexDCA and the legacy user interface?
The :SYSTem:FCONfig command can be used to switch between the possible user interfaces.

FAQ 2013-12-12

我可以連續頻率頻帶操作 86107A 嗎?
若 86100A/B/C 主機具備 A04.10 版或更新版的韌體,便可以下列連續頻率範圍操作 86107A。

FAQ 2013-12-12

1 2 3 4 5 6 7 8 9 10 ... 下一頁