Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

76-100 из 414

Упорядочить:
For the InfiniiMax probes, what effect does the "Signal being probed" setting have? Why do I have to specify single-ended or differential?
Infiniium scopes and InfiniiMax differential probe amplifiers have a unique method of applying DC offset which considers whether the signal being probed is single-ended or differential...

FAQ 2010-10-06

86100A/B/C Infiniium DCA Firmware Upgrades
86100A/B/C Infiniium DCA Firmware Upgrades

FAQ 2010-09-23

86100C DCA-J - TDR/TDT Mode
86100C DCA-J - TDR/TDT Mode

FAQ 2010-09-21

Can the 6000 Series oscilloscopes make floating measurements?
Like most other digitizing oscilloscopes, the new 6000 Series is not designed to offer floating measurement by itself. With 6000 Series you can make floating or differential measurements using a differential probe.

FAQ 2010-09-20

How do I save a screen image from my 5000/6000/7000-series InfiniiVision oscilloscope to a USB storage device?
These instructions assume that your scope has system software version 05.00 or later (see Utility | Service | About Oscilloscope -> System version to see your scope’s version).

FAQ 2010-09-15

How do I extract the 32Mpts from U270xA?
One way of “viewing” the full memory waveform is using the zoom function (that the red arrow...

FAQ 2010-09-14

VEE Pro: Why can't I talk to an instrument at GPIB address 21?
The reason is that each device on the GPIB has to have a unique address, including the computer's GPIB card.

FAQ 2010-09-09

How do I get my Infiniium to recognize new daylight savings time dates?
For Infiniium oscilloscopes with the Windows® XP operating system, you can download an update from Microsoft ...

FAQ 2010-09-08

Why can't I purchase the 11899A Probe Power Supply for my 85024A, Active Probe?
11899A is no longer supplied, see details for alternative solution...

FAQ 2010-08-18

When I press the Power On button on my U1602A/U1604A Handheld Oscilloscope, it does not boot up. Instead, the screen just flashes …
To turn on your U1602A/U1604A Handheld Oscilloscope, you will need to press and hold the Power On button for approximately 3 seconds….

FAQ 2010-08-09

In the programming for the U2701A and U2702A Modular Oscilloscopes, why do I sometimes get a different waveform…
In programming the U2701A/U2702A Modular Oscilloscopes, the waveform is different from the Measurement Manager's (AMM) because....

FAQ 2010-08-09

When using the U1602A/U1604A Handheld Oscilloscope, I can see an offset value at the vertical axis although there is no connection…
When you see an offset value at the vertical axis although there is no connection at the test probe, try running the self-calibration….

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why does the pulse shape of my scope probe compensation look different from the pulse shape shown…
The compensation signal (square wave) that you see is different from the pulse shape shown in the U1602A/U1604A's user’s manual because….

FAQ 2010-08-09

Why does the new U1571A battery pack for my U1602/4A Handheld Oscilloscope last less than the stipulated 4 hours…
The new U1571A battery pack of the U1602A or U1604A Handheld Oscilloscope lasts less than 4 hours because….

FAQ 2010-08-08

How do I convert *.svw file to *.csv file in PC Link for U160xA/B?
1) From within PC Link, click on the "Load SVW" icon on the tool bar...

FAQ 2010-07-18

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

I misplaced the scope’s hostname, what would I do to reset the hostname?
To reset the hostname, follow these instructions.

FAQ 2010-07-02

What replaceable parts are available for the E5383A 17-channel single-ended flying lead set?
The lead set, IC clips, probe leads, ground leads, and common (long) ground leads are available for individual purchase.

FAQ 2010-07-02

I have purchased the Segmented Memory option, N5454A, for my InfiniiVision oscilloscope. However, I can’t find the feature in the menus. What can I...
You need to upgrade your oscilloscope to the latest firmware...

FAQ 2010-07-02

What is the use model? Charge as much as possible or let it run down, then charge all the way up?
It’s not necessary to run all the way down like NICAD battery.

FAQ 2010-07-02

In the user calibration of InfiniiVision 5000/6000/7000 Series oscilloscopes, what accessories are needed, and what is the procedure?
Here are the required accessories, and the procedure is at ...

FAQ 2010-06-08

What replacement parts and accessories are available for the 113xA-series InfiniiMax probes?
The best place to find this information is in the most recent revision of the InfiniiMax Active Probes User´s Quick Start Guide.

FAQ 2010-06-07

Infiniium Oscilloscopes: SCPI compliance

FAQ 2010-05-16

How do the :MEASure:SENDvalid and :MEASure:STATistics commands affect my Infiniium's measurement results?

FAQ 2010-05-16

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие