Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

26-50 из 414

Упорядочить:
What are the remote control commands to switch between FlexDCA and the legacy user interface?
The :SYSTem:FCONfig command can be used to switch between the possible user interfaces.

FAQ 2013-12-12

Can I operate 86107A over continuous frequency bands?
The 86107A can operate over the following continuous frequency range if the 86100A/B/C mainframe has firmware revision A04.10 or above.

FAQ 2013-12-12

Can I upgrade my 86100A, 86100B or 86100C mainframe to obtain an 86100D?
The 86100D has major hardware differences that make an upgrade uneconomical. Keysight regularly offers trade-in and other incentive programs for DCA mainframes. Contact your local representative for details about the current trade-in program available for your unit.

FAQ 2013-11-27

Why does handheld scope’s date/time display disappears or shows hexa characters?
This condition indicates that the internal memory battery level is low.

FAQ 2013-11-22

Can I upgrade to option 001(Host USB interface) for the U1600A Series Handheld Oscilloscopes after purchase?
No, you cannot upgrade to option 001 for the U1600A Series Handheld Oscilloscopes after purchase….

FAQ 2013-11-17

Are the input channels on the U1602A and U1604A Handheld Oscilloscopes isolated?
No, the scope channels 1 and 2 on the U1602A and U1604A Handheld Oscilloscopes are not isolated. They share the same ground.

FAQ 2013-11-17

Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....

FAQ 2013-11-17

Can I switch off the U1602A/U1604A Handheld Oscilloscope's audible key sound?
Yes, you have the option to switch on or off the audible key sound of the U1602A/U1604A Handheld Oscilloscope….

FAQ 2013-11-17

Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

What parts and accessories are available for my 10400A-series probe?

FAQ 2013-11-15

Why is the segmented memory acquisition mode useful and which Infiniium oscilloscopes support it?
Segmented memory mode offers more efficient acquisition memory usage for storing waveforms with events of interest that are separated by long periods of time. All currently shipping Infiniiums and many older units support segmented memory.

FAQ 2013-09-18

How to install the U2701A/U2702A IVI driver on Windows 10?
Yes, but you need to run a special command after installation...

FAQ 2013-07-20

Infiniium Oscillscopes: Trigger Setup for Violation Mode
When triggering on a setup time violation, what would cause a trigger to occur on a setup time value that is larger than specified?

FAQ 2013-05-31

Infiniium Oscilloscopes: Mouse and Trackball Usage
What type of mouse can be used with the Infiniium oscilloscope? Can a trackball device be used?

FAQ 2013-05-31

Infiniium Oscilloscopes: Waveform Labeling
Is it possible to label waveforms?

FAQ 2013-05-31

How can I bundle N1045A remote heads together in a tight space?
For simple differential setups, two heads can simply be clipped together using the supplied clip. To mount more heads see the full body of this FAQ for mounting dimensions and thermal considerations.

FAQ 2013-04-24

What are the rack mount kit part numbers for the 86100 DCA?
Rack mount kits for 86100 DCA are available to purchase as stand-alone parts.

FAQ 2012-12-20

Can I remotely query the 86100D DCA-X to determine which user interface is running?
Yes. Issue the query :SYSTem:FCONfig? If the response is "Legacy" then the legacy UI is in use. If the response is "Compatible" or "Standard" then the FlexDCA interface is in use.

FAQ 2012-12-12

How do I order the Infiniium oscilloscope hard drive replacement kit?
For Infiniium oscilloscopes with the Windows® XP operating system, the part number depends on the oscilloscope model number ...

FAQ 2012-11-13

Does Keysight offer any application notes that discuss the theory of Time Domain Reflectometry (TDR) measurements?
Keysight provides Application Note 1304-2, "Time Domain Reflectometry Theory".

FAQ 2012-11-05

Can I manually set the sample rate on my InfiniiVision oscilloscope?
Although the sample rate cannot be directly set on any InfiniiVision oscilloscope, it can be set indirectly by adjusting the oscilloscopes time per division setting.

FAQ 2012-10-30

Which Keysight oscilloscopes have a 10 MHz reference input/output?
6000 Series, 6000L Series, 7000A Series, 7000B Series, 9000 Series, 54850 Series (Output only), 80000A Series, 80000B Series, 90000A Series and 90000 X-Series

FAQ 2012-10-17

What is the difference between the Auto and Normal trigger modes on InfiniiVision oscilloscopes?
In auto trigger mode, the trigger will be forced if the specified conditions are not met. In normal trigger mode, the trigger will never be forced and a trigger will only occur if the specified conditions are met.

FAQ 2012-10-17

All IntuiLink Tools for Keysight Oscilloscopes
Supported Models: Infiniium Series, 1000 Series, 2000 X-Series, 3000 X-Series, 5000 Series, 6000 Series, 7000 Series, and 54600 Series Oscilloscopes

FAQ 2012-09-26

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие