検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

コンテンツのタイプ

製品カテゴリ

1-25 / 745

並べ替え
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

Infiniium Oscilloscope Software
Infiniium oscilloscope software.

FAQ 2019-08-08

Are there 3D models of the Infiniium UXR-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2019-02-19

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

Is there a 3D model of the P9241A USB oscilloscopes?
Yes, see the IGES, Step, and PKG format file downloads.

FAQ 2018-09-21

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-07-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

XY Display Mode Example
The XY time mode converts the oscilloscope from a volts-versus-time display to a volts-versus-volts display using two input channels.

FAQ 2017-02-24

最高の低価格オシロスコープをお探しですか?
Keysight InfiniiVision 1000 Xシリーズ50~100 MHzオシロスコープは、専門的な品質の機能を今までにない低価格で提供します。

FAQ 2017-02-07

Is there a 3D model of the Infiniium V-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2017-01-25

Infiniium Oscilloscope HDD/SDD in Secure Environments
This FAQ talks about how to deal with Infiniium oscilloscope HDD/SDD in secure environments if you need to send oscilloscopes in for calibration.

FAQ 2016-09-26

Is there a 3D model of the InfiniiVision 6000L Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2016-07-18

Which printers are supported by the handheld oscilloscopes?
Keysight handheld oscilloscopes support PCL6, 5e,5c and Postscript level 3 emulation printer command languages.

FAQ 2015-11-09

Infiniiumオシロスコープ基本操作&測定手順のビデオ
YouTubeビデオで操作/測定手順をご覧頂けます。

FAQ 2015-04-24

Keysight License Managerを使用したライセンスの移行手順は?
Keysight License Managerを使用したライセンスの移行手順をご覧ください。

FAQ 2015-03-12

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Does the 86100D DCA-X Support Windows 7?
Yes. Existing mainframes my be upgraded by ordering 86100DU-WN7 from your local contact center. All the new 86100Ds ship with Windows 7 installed.

FAQ 2014-09-25

既に販売が完了したKeysight、AgilentおよびHewlett-Packard(HP)のテスト機器のマニュアルはどのように入手できますか?
ほとんどのKeysight製品にPDFマニュアルがあり、製品ページで入手することができます。Keysightのベンダも古いマニュアルを提供しています。

FAQ 2014-08-01

Windows XPサポート終了に伴う 、Windows7への対応は?
Windows XPからWindows7へのアップグレード品を用意したり、後継機種をご案内したりしています。計測器の価値を保ち、継続的してご利用いただくため、ご対応をお勧めします。

FAQ 2014-05-07

Is there a 3D model of the InfiniiVision 6000 X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2014-04-29

1 2 3 4 5 6 7 8 9 10 ... 次へ