Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 52

Sort:
How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Can a CalPod system be used with the N1500A software?
No, the CalPod and N1500A Software are not compatible.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

For signals requiring wider bandwidth, how can Keysight’s LTE Signal Studio waveform creation products be used to increase carrier spacing?
Set the FFT length to 8192 and a sample rate of 800 MHz. Subcarrier spacing = sampleRate/FFT size

FAQ 2017-06-28

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

How can the E6650A EXF sequencer help to accelerate my testing speed?
The sequence analyzer is an evolution from traditional measurement method.

FAQ 2014-09-08

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

Comparisons of GNSS Solutions
View this table for product comparisons.

FAQ 2014-03-25

What is 802.11af, and does Keysight have a solution for testing 802.11af devices?
Learn more about Keysight's 802.11af solutions…

FAQ 2014-02-28

How does the 89601BU "update and subscription service" work?
Option 200 is mandatory and you cannot use the 89600 VSA software without having Option 200 installed. Software version.....

FAQ 2014-01-27

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

Are there any options to adjust the pulse definitions within Signal Studio for pulse building?
No, at the moment the rise and fall times are defined by their 0-100 percent points and the pulse width is defined to be the 100-100 percent point.

FAQ 2013-05-16

How do I change the 10 MHz reference source if Signal Studio for pulse building doesn’t detect the reference?
Most of the time, Signal Studio will recognize the reference; however, it can be changed in the download -> customize menu.

FAQ 2013-05-16

Is it possible to adjust the phase offset using degrees instead of radians?
Yes. Select View -> Customize Pattern Item Table and toggle the ‘phase offset in degrees’ button

FAQ 2013-05-16

Is there a way to put insert a missing pulse into the signal?
Yes, you can add a “Off time” object to the pulse pattern and change the duration to meet your pulse requirements.

FAQ 2013-05-16

When I use the 30-day trial license of the Signal Studio for WiMAX™, how can I check the number of days remaining on temporary license?
Press the front panel keys: Utility > Instrument Adjustments > Instrument Options > Waveform Licenses

FAQ 2013-01-28

Is there a way to simulate jitter in my pulse pattern?
Yes, Signal Studio for pulse building allows you to add jitter on the pulse width and pulse repetition interval.

FAQ 2012-12-30

Does the Signal Studio for Pulse Building software run on a National Instruments embedded PXI controller like the one that comes with the N6030A?
Yes, it does. However, the Keysight I/O Libraries may need to be installed as a secondary VISA and then the NI Tulip DLL may need to be enabled.

FAQ 2012-12-30

Is there an easy way to save a pulse pattern and send it to another person?
Yes, simply save the entire .pbp or you can export the pattern using the “export pattern” function.

FAQ 2012-12-30

When would I use ALC Hold?
ALC Hold is used for pulses with rise and fall times greater than 100 ns. It is used with pulses that do not have constant envelope modulation (such as AM Step), and with multiple pulses where the pulses have different amplitudes.

FAQ 2012-12-30

Can I turn off the N6030A arbitrary waveform generator predistortion from the N7620B Signal Studio for Pulse Building to get more power?
No. The N7620B software does not allow the N6030A predistortion to be turned off.

FAQ 2012-12-30

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

What is the internal Arb trigger delay jitter?
The internal Arb trigger delay is generated using a free running oscillator.

FAQ 2012-12-28

How many coefficients should I use for custom FM?
The number of coefficients to use depends on the type of custom FM signal desired. Signal Studio for Pulse Building includes examples where 19 coefficients were used. The software allows as many coefficients as desired. The more coefficients used,...

FAQ 2012-12-28

1 2 3 Next