Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

Categoria de Produto

1-2 de 2

Sort:
What is the PRBS (pseudo random binary sequence) polynomial used to test BER in the DVB-T/H system?
The PRBS, which is in compliance with ITU-T O.151, is based on the generator polynomial, 2e23–1 or 2e15–1.

FAQ 2010-02-05

For Xilinx FPGA Dynamic Probe, when should I use Xilinx Core Generator instead of Core Inserter?
Core Generator is usually preferable if you need partitions, since Core Inserter does not support partitions. Core Generator does support partitions but is much less convenient.

FAQ 2010-01-24