您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-2 / 2

排序:
What is the PRBS (pseudo random binary sequence) polynomial used to test BER in the DVB-T/H system?
The PRBS, which is in compliance with ITU-T O.151, is based on the generator polynomial, 2e23–1 or 2e15–1.

FAQ 2010-02-05

For Xilinx FPGA Dynamic Probe, when should I use Xilinx Core Generator instead of Core Inserter?
Core Generator is usually preferable if you need partitions, since Core Inserter does not support partitions. Core Generator does support partitions but is much less convenient.

FAQ 2010-01-24