您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 144

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How does the Microsoft end of support for Windows XP affect my B1500A and B1505A Device Analyzer?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will provide the information about the migration from Window XP to Windows 7.

FAQ 2014-04-30

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Can the B2900A Series of SMU sweep voltage source by the know on the front panel?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-09-16

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

Can I use N1294A-021/022 low noise filters with B2901A/02A/11A/12A SMU?
No, they aren't recommended to be used with the Keysight B2901/02/11/12A SMUs.

FAQ 2013-09-16

How can the B2900A Series of SMU source pulses whenever it receives an external trigger signal?
It can do it by configuring a digital I/O pin to be used for an external trigger signal. Click the above link for details.

FAQ 2013-09-16

Does the B2900A Series of SMUs have Source Memory Sweep Function?
No, the B2900A Series of SMUs doesn't have Source Memory Sweep Function as Keithley 2400 has.

FAQ 2013-09-16

How to use the interlock to output more than ±42V?
B2900A has interlock detection with the digital I/O on the rear pannel. Click the link for details.

FAQ 2013-09-16

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

How can I set up Power-on State of the B2901/02/11/12A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2012-11-21

Can I use the triaxial cable with B2900A?
Yes. You can use the triaxial cable by using the N1294A adaptor.

FAQ 2012-11-20

Does the B2901/02/11/12A have any search function?
No, the B2901/02/11/12A doesn't have any search function which the analyzers such as the B1500A have.

FAQ 2012-10-09

The channel 2 in the B2902A or B2912A doesn't receive any SCPI commands.
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

I cannot store the channel 2 measurement condition to USB memory stick, why not?
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

The password is required to access the instrument.
The password is required to access the instrument compliant with the LXI specification. Click the above link for details.

FAQ 2012-10-09

How to determine the frequency for Sin function of Quick IV List Sweep?
Frequency = 1 / ( (360 [degree] / X Step [degree]) * Trigger Period )

FAQ 2012-10-09

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

How many capacitance measurement units (MFCMUs) can be installed in the B1500A?
Only one MFCMU can be installed in a B1500A mainframe.

FAQ 2012-06-07

How can I configure to output continuous arbitrary waveform?
Click the above link for details.

FAQ 2012-03-26

How can I find the power-on program setting of the B2901/02/11/12A?
You can find the power-on program setting on the System Start-up dialog box. Click the above link for details.

FAQ 2012-02-01

How to configure the time constant of the output filter with the B2901/02/11/12A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2012-02-01

1 2 3 4 5 6 下一頁