Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-6 of 6

Sort:
Why isn’t the screen bigger?
The screen is optimized for the “typical” engineering environment where the instrument is up on a lab desk you need to read the numbers from the screen from any angle. In case you need a bigger screen you can manage and control the instrument from...

FAQ 2008-02-21

What does channel add mean?
You can add the signal from one channel to the signal of the other channel this might be adding noise to a clean pulse, this might be a FM signal added with noise… The possibilities you have are huge.

FAQ 2008-01-29

What is a crest factor?
The crest factor defines the ratio between Vp to RMS. The ideal sine wave for example has a crest factor of 1.414. Any crest factor higher than 1.414 shows additional noise, distortion or spikes. In addition the crest factor shows signal boundar...

FAQ 2008-01-29

I have a Keysight Pulse Generator, Why shall I buy this new instrument?
In addition to Keysight’s proven Pulse Generator the 81150A provides distortion & modulation capabilities. This gives you complete new test possibilities. In addition the instruments provides coupling & uncoupling of channels. With the coupling you...

FAQ 2008-01-29

Why are you offering 3 instruments in 1? What if my customer needs only one of these instruments?
In addition to precise pulses and trigger customers need to stress the device to its limits. In the past they used either a second channel or an additional instrument to distort the signal. With the new build-in capabilities real-world signals can...

FAQ 2008-01-29

How to upgrade from 1 to 2 channels
It is not possible to upgrade a 1 channel version to a 2 channel version. You have to decide from the beginning how many channels you need.

FAQ 2008-01-29