您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 755

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

Signal Generator Firmware Update Center
Download signal generator firmware, release notes, upgrade guide and FAQs.

FAQ 2019-07-19

M8000 系列軟體 30 天免費試用授權
M8000 產品系列適用的軟體之試用授權頁面與連結。

FAQ 2019-05-21

How do I upgrade my N5166B CXG Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2019-04-26

Why is readback voltage/current different from actual value when the recall function is used after power cycling the unit?
Users may encounter incorrect voltage/current readback reading under the following conditions

FAQ 2019-02-27

Signal Generator (Signal Source) Upgrade Center
Information to perform a signal generator upgrade or signal source upgrade.

FAQ 2018-06-19

M8020AU Upgrades for J-BERT M8020A high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option

FAQ 2017-12-13

Signal Analyzer LabVIEW Instrument Drivers
Supported models: N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, N8973B, N8974B, N8975B, N8976B, M8920A

FAQ 2017-12-01

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

利用現代化桌上型電源供應器節省測試時間
是德科技新的經濟型直流桌上型電源供應器具有獨立的三路輸出和內建的資料記錄器。了解現代化桌上型電源供應器如何協助您。

FAQ 2017-06-20

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

如何找到儀器或 PC 的主機 ID(HOST ID)?
是德科技軟體選項已獲得許可,可將唯一的硬體識別符(主機 ID)用於各種不同類型的硬體。取決於軟體型號和目標硬體平台,主機 ID 由 1、2 或 3 個元素組成。

FAQ 2016-05-23

How do I clear the External Reference Warning on the display?
Step by step procedure can be found here...

FAQ 2016-01-08

How do I set the reference to external, have notification of any external reference problems, and have it remain external with a Preset?
Process steps included here...

FAQ 2016-01-08

How do I upgrade my N5191A UXG X-Series Agile Signal Generator, Modified Version, 10 MHz to 40 GHz?
Find Information on Hardware Upgrades, Instrument Software, etc.

FAQ 2015-10-01

For an auto-ranging power supply, how do I determine the maximum output current for any operating voltage? | Keysight
You will always obtain rated output power of the unit along any point of the auto-ranging operating curve.

FAQ 2015-09-08

How do I upgrade my N5182B MXG Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2015-04-22

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

1 2 3 4 5 6 7 8 9 10 ... 下一頁