Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

retirer tout le raffinement

Par sujet

Par type de contenu

Par catégorie de produit

1-25 sur 110

Tri:
How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

What is the P/N of cable between E4980A and 42841A?
The current cable is p/n E4980-61640.

FAQ 2014-02-06

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

What mechanical calibration kits and ECal (electronic calibration) kits does the ENA support?
Please refer to following documents...

FAQ 2012-12-11

Can I use the 16092A with the 4395A/4396B/4287A/E4991A?
Yes, you can use the 16092A with the 4395A/4396B/4287A/E4991A.

FAQ 2012-05-10

What is the recommended transit case for my Keysight ENA Series Network Analyzer?
Custom fit ENA Series transit cases are not available. However customer can refer to other commercial company’s product like Pelican or ECS case.

FAQ 2012-02-28

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

Is there an error in the delay/thru definition for the 85039B F-Type Calibration Kit?
Yes.

FAQ 2011-10-07

Are the adapters in the 85033E 30kHz to 9GHz calibration kit phase matched?
Yes.

FAQ 2011-10-07

Does the ENA contain parts with limited service life?
Yes.

FAQ 2011-10-07

How can I find accessories for a Keysight product?
For instrument-specific accessories (such as probes for an oscilloscope), first go to the product page and then see the related accessories. For general-purpose accessories (such as rf & microwave test accessories, carts, and racks), go to the ...

FAQ 2011-10-07

Why is the "E-230 data corrupt or stale" error message occasionally displayed on the E4980A while saving a measurement data in the USB memory stick...
It is caused when the procedure for saving a data is not performed correctly or when the USB memory stick is not compatible with the E4980A.

FAQ 2011-07-24

What is a recommended USB memory device for the E4980A and the E4981A?
4 GB USB Memory (Keysight PN 1819-0637) is recommended.

FAQ 2011-07-11

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?
Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment.

FAQ 2011-06-07

What is the interface cable or adapter required to control external GPIB equipment by using VBA macro function of the E4991A?
The 10833A/B/C/D, 82357A or 82357B is required depending on the OS version of the E4991A.

FAQ 2011-06-07

Why is permeability measurement result unstable when a low permeability magnetic material or a thin magnetic material is measured with the 16454A?
It is because the impedance of the magnetic material inserted into the 16454A is too low for the impedance analyzer to measure it accurately.

FAQ 2011-06-07

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?
No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can be used with the 4338A/B only.

FAQ 2011-06-07

Can the 42941A probe be used with any RF test fixture adapter?
No, the 42941A does not have any test fixture adapter available for connecting the probe to an RF component test fixture.

FAQ 2011-06-07

Can the 42941A probe be substituted for discontinued 41941A/B probe?
No, the 42941A cannot be substituted for the discontinued 41941A/B and doesn’t have compatibility with old 4194A analyzer.

FAQ 2011-06-07

How should a DC blocking capacitor be inserted between the 42941A probe and a DUT when a live DC voltage exists on the device?
It is recommended to insert a SMA DC blocking adapter between the furnished pin probe and 3.5-mm connector at the tip of the 42941A.

FAQ 2011-06-07

What additional items are required to utilize the E4991A option 007 Temperature Characteristic Test Kit?
For newly purchased E4991As a Keysight 82357B USB-GPIB card is required as well as a GPIB interface on the temperature chamber. The recommended temperature chamber is an ESPEC model SU-261 temperature chamber.

FAQ 2011-05-31

Is there any effective way to measure the impedance of a pressure sensitive SMD component (ex. a ferrite bead) with the 16196 series or 16197A test...
In order to measure a pressure sensitive device, the pressure applied to the DUT by the test fixture needs to be carefully controlled.

FAQ 2010-07-02

Can the cylindrical insulator reduce the effect of magnetic coupling between the inductive DUT and the outer conductor of the 16196A/B/C/D fixtures...
Yes, but the effect of reducing the magnetic coupling effect is not sufficient and depends on the DUT.

FAQ 2010-07-02

How can I connect a test fixture to the measurement terminals of the E4980A when the stopper at the rear of the fixture disturbs the connection?
Remove the stopper from the test fixture by removing a screw at the center of the plastic stopper. Otherwise, remove the front rubber guide from the E4980A.

FAQ 2010-07-02

1 2 3 4 5 Page suivante