您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-25 / 110

排序:
How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

E4980A 和 42841A 之間的纜線的產品編號是什麼?
目前的纜線的產品編號是 E4980-61640。

FAQ 2014-02-06

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

What mechanical calibration kits and ECal (electronic calibration) kits does the ENA support?
Please refer to following documents...

FAQ 2012-12-11

是德 ENA 系列網路分析儀適合使用什麼樣的提箱?
Keysight ENA 系列提箱沒有專屬的提箱。客戶仍可參考其他公司生產的提箱,如 Pelican 或 ESC 提箱。

FAQ 2012-03-12

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

Keysight 85033E 30kHz 到 9GHz 校驗套件中的轉接器是與相位匹配的嗎?
是的。

FAQ 2011-10-07

Does the ENA contain parts with limited service life?
Yes.

FAQ 2011-10-07

如何找到是德產品的配件?
如需特殊儀器配件(例如示波器用測試探棒),請先到產品網頁,然後查看相關的配件。

FAQ 2011-10-07

85039B F型校驗套件的延遲/貫穿定義中是否有錯誤?
定義值中沒有錯誤,但您在量測插入待測裝置時,必須修改定義值。

FAQ 2011-10-07

進行將量測資料儲存於 USB 隨身碟中的操作程序時,Keysight E4980A 上為什麼偶而會顯示「E-230 data corrupt or stale」錯誤訊息?
若未正確儲存資料,或 USB 隨身碟與 Keysight E4980A 不相容時,會顯示這項錯誤訊息。

FAQ 2011-07-24

What is a recommended USB memory device for the E4980A and the E4981A?
4 GB USB Memory (Keysight PN 1819-0637) is recommended.

FAQ 2011-07-11

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?
Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment.

FAQ 2011-06-07

What is the interface cable or adapter required to control external GPIB equipment by using VBA macro function of the E4991A?
The 10833A/B/C/D, 82357A or 82357B is required depending on the OS version of the E4991A.

FAQ 2011-06-07

Why is permeability measurement result unstable when a low permeability magnetic material or a thin magnetic material is measured with the 16454A?
It is because the impedance of the magnetic material inserted into the 16454A is too low for the impedance analyzer to measure it accurately.

FAQ 2011-06-07

Can the 16338A be used with LCR meters such as the 4263B and the E4980A?
No, the 16338A Test Lead Set doesn’t have compatibility with LCR meters. The 16338A can be used with the 4338A/B only.

FAQ 2011-06-07

Can the 42941A probe be used with any RF test fixture adapter?
No, the 42941A does not have any test fixture adapter available for connecting the probe to an RF component test fixture.

FAQ 2011-06-07

Can the 42941A probe be substituted for discontinued 41941A/B probe?
No, the 42941A cannot be substituted for the discontinued 41941A/B and doesn’t have compatibility with old 4194A analyzer.

FAQ 2011-06-07

How should a DC blocking capacitor be inserted between the 42941A probe and a DUT when a live DC voltage exists on the device?
It is recommended to insert a SMA DC blocking adapter between the furnished pin probe and 3.5-mm connector at the tip of the 42941A.

FAQ 2011-06-07

若要運用 E4991A 選項 007 溫度特性測試套件,還需要什麼另外的配件?
新購的 Keysight E4991A 需搭配使用 Keysight 82357B USB-GPIB 卡,同時溫度測試機也需配備 GPIB 介面。 我們推薦使用的溫度測試機是 ESPEC model SU-261 溫度測試機。

FAQ 2011-05-31

Can the cylindrical insulator reduce the effect of magnetic coupling between the inductive DUT and the outer conductor of the 16196A/B/C/D fixtures...
Yes, but the effect of reducing the magnetic coupling effect is not sufficient and depends on the DUT.

FAQ 2010-07-02

How can I connect a test fixture to the measurement terminals of the E4980A when the stopper at the rear of the fixture disturbs the connection?
Remove the stopper from the test fixture by removing a screw at the center of the plastic stopper. Otherwise, remove the front rubber guide from the E4980A.

FAQ 2010-07-02

Do the coaxial Short and 50 Ω Load terminations for the 42941A have accuracy specifications?
No, both the coaxial Short and 50 Ω Load standard terminations for the 42941A do not have accuracy specifications.

FAQ 2010-07-02

Can I separately order the heat-resistant cable without ordering E4991U-007 Upgrade Kit?
No. The heat-resistant cable cannot be ordered separately from the E4991U-007.

FAQ 2010-07-02

1 2 3 4 5 下一頁