Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

1-25 de 526

Sort:
The temperature characteristic test sample program does not work on the 64-bit version of Excel.
Download and use the Tctest64.xlsm

FAQ 2019-08-21

How do I upgrade my E4990A Impedance Analyzer?
Information for hardware and software options upgrade

FAQ 2019-02-24

How do I upgrade my E5061B ENA Series Network Analyzer?
Information for hardware and software options upgrade

FAQ 2018-11-08

What is the CPU / Storage / Windows OS history?
The history of CPU type/memory size, storage type/size, windows OS is listed in the table.

FAQ 2018-08-21

Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

Where can I find information on E4980A/AL error messages?
E4980A/AL error messages are described in Appendix B of the Users Guide.

FAQ 2017-06-28

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

How do I upgrade my 4396B Network/Spectrum/Impedance Analyzer?
Information for hardware and software options upgrade

FAQ 2016-02-26

What is enhanced overload detection and power trip function?
Since the autumn in 2015, the E5061B Option-115/117/135/137/215/217/235/237 ships with enhanced overload detection and power trip function. The E5061B Option-3L5 does not have this function.

FAQ 2016-01-28

How does the Microsoft end of support for Windows XP affect my ENA?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will help you answer some important questions.

FAQ 2015-07-27

How do I upgrade my E4991B Impedance Analyzer?
Information for hardware and software options upgrade

FAQ 2015-06-19

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

How can I make 75 Ω measurements using the ENA?
You can make 75 Ω measurements with the ENA by shifting system characteristic impedance to 75 Ω.

FAQ 2015-03-09

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How do I upgrade my E4982A LCR Meter?
Information for hardware and software options upgrade

FAQ 2014-05-01

How does the Microsoft end of support for Windows XP affect my E4982A?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will help you answer some important questions.

FAQ 2014-04-24

What are the differences between the E4980A and 4284A?
Most of the E4980A functions are compatible with the 4284A's. Since some enhancements and updates of functionality are incorporated in the E4980A, there are primary differences summarized in the table.

FAQ 2014-04-07

Can you advise of alternatives to printing and acquiring screen images from the various Keysight Analyzers equipped with only a GP-IB interface?
There are several way to retrieve screenshots.

FAQ 2014-02-18

What is the P/N of cable between E4980A and 42841A?
The current cable is p/n E4980-61640.

FAQ 2014-02-06

Replacing the 8508A vector voltmeter with the E5061B network analyzer
Measuring the phase difference of an external CW signals is a typical measurement application of the 8508A vector voltmeter.

FAQ 2013-10-14

How can I order the upgrade kit of the 4395A
The model numbers of available upgrade kits for the 4395A options are as follows.

FAQ 2013-06-24

1 2 3 4 5 6 7 8 9 10 ... Avançar